Freemaster Recorder Memory Allocation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster Recorder Memory Allocation

1,901件の閲覧回数
duanemattern
Contributor III

I'm using Freemaster on an old dsp56805 board. I have it working, can display, plot, log data, and now I'm attempting to use the recorder capability for high speed data collection.  When I setup the variable to record, it tells me I've only 36 bytes and can only collect 18 samples of this 2-byte variable.    I attempted to change the PCMASTER_REC_BUFFER_LEN (on old implementation), but I don't see any change to the available memory.  I've read through several documents and don't see a description on how to adjust the size of the memory available to the recorder.  Any suggestions would be appreciated.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,721件の閲覧回数
duanemattern
Contributor III

Never mind. I was making the change in the wrong location.  #defines assigned in appconfig.h in my application.

0 件の賞賛
返信