FreeRTOS - MPC5748g - DevKit.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS - MPC5748g - DevKit.

4,871 Views
Krishnaja
Contributor II

Hi,

To a "freertos_mpc5748g" example, I added a "linflexed_uart" component. And also created a task for linflexed_uart.
But I am not getting linflexed_ uart task output.

Krishnaja.

0 Kudos
Reply
10 Replies

4,834 Views
Krishnaja
Contributor II

Hi Lukas,

I don't think timeout is an issue. Anyways I tried as you suggested by keeping the value to 3seconds. But it did not help.

I had created the return code for linflexed uart task, just below led task.

I am using S32 Design Studio for power Architecture Version2.1 .

Can you go through the code and tell me what I have missed.

 

Krishnaja.

 

0 Kudos
Reply

4,846 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

isn't the timeout value of LINFLEXD_UART_DRV_ReceiveDataBlocking function too short?

What is the return code of this function? I can see you don't check it.

If this doesn't help, what is the version of SDK and S32DS?

Regards,

Lukas

 

 

0 Kudos
Reply

4,780 Views
Krishnaja
Contributor II

Any updates?? @lukaszadrapa 

Tags (1)
0 Kudos
Reply

4,772 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

sorry for delay, we had Easter holidays here, so some answers are delayed.

Let me repeat this question to move forward - what is the return code from LINFLEXD_UART_DRV_ReceiveDataBlocking?

Regards,

Lukas

 

0 Kudos
Reply

4,767 Views
Krishnaja
Contributor II

 

Hi,

Let us keep receive Data block aside for time being. 

I have attached main of my code. According to high-lighted code, I should get "Hello world!" msg before the scheduler task on terminal. But I am not getting the same.

int main(void)
{


/* Write your local variable definition here */
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
#ifdef PEX_RTOS_INIT
PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of Processor Expert internal initialization. ***/
/* Initialize clocks */
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
/* Initialize LINFlexD module for UART usage */
LINFLEXD_UART_DRV_Init(INST_LINFLEXD_UART1, &linflexd_uart1_State, &linflexd_uart1_InitConfig0);
/* Send the greeting message to console */
LINFLEXD_UART_DRV_SendData(INST_LINFLEXD_UART1, (uint8_t*)msg, strlen(msg));


#if START_OS_DEMO
/**/
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)4, mainLED_TASK_PRIORITY, NULL );
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)1, mainLED_TASK_PRIORITY+1, NULL );
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)2, mainLED_TASK_PRIORITY+2, NULL );
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)3, mainLED_TASK_PRIORITY+3, NULL );

xTaskCreate( uartTask, ( const char * const ) "UARTTask", configMINIMAL_STACK_SIZE, (void*)0, mainLED_TASK_PRIORITY+4, NULL );

//ptr to entry fn(name of fn),descriptive name of task(debugger),no of words, value passed to create task, priority, optional
/* Start the scheduler. */
vTaskStartScheduler();
#endif

 

Krishnaja.

Tags (1)
0 Kudos
Reply

4,748 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

could you send me whole project? I'm afraid the main is not enough in this case.

Thanks,

Lukas

 

0 Kudos
Reply

4,727 Views
Krishnaja
Contributor II

Hi,

PFA

 

Regards,

Krishnaja.

0 Kudos
Reply

4,710 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

It is mandatory to call init and other functions (if drivers uses OS services) after starting scheduler. Otherwise it won't work.

Regards,

Lukas

 

 

0 Kudos
Reply

4,692 Views
Krishnaja
Contributor II

Hi,

Tell me how to call init and what other functions should i call and where?

 

Krishnaja.

0 Kudos
Reply

4,665 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply