Flexray Communication error:

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexray Communication error:

2,007件の閲覧回数
sumanth
Contributor I

Hello,

I'm using MPC5607B controller (XPC56XX EVB motherboard with XPC5607B daughter), trying to implement Flexray communication using sample "Flexray unified driver MPC560xP", but facing an issue in API,   Fr_return_type Fr_init(const Fr_HW_config_type *Fr_hw_config_temp_ptr, const_Fr_low_level_config_type *Fr_low_level_config_temp_ptr) {

 

The following Condition is not satisfied,

 

while( I < FR_MAX_WAIT_CYCLES)&& ((Fr_CC_reg_ptr[FrPSR0] & 0x700U)  ! =  FrPSR0_PROSTATE_CONFIG))

 

and Fr_init is  Failed.

 

Please provide inputs..

ラベル(1)
0 件の賞賛
返信
1 返信

1,750件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there's no FlexRay module on MPC5607B.

Regards,

Lukas

0 件の賞賛
返信