FlexRay : FR_MBIDXRn[MBIDX] register value changes after frame reception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexRay : FR_MBIDXRn[MBIDX] register value changes after frame reception

1,626 Views
Deepak1
Contributor IV

Hi,

I am using DEVKIT MPC5748G development Board for FlexRay driver development and IDE is S32 DS for power architecture V2.1.

I am stuck in a problem and need your suggestions to come out from this.

Node 1 : Transmitter

Node 2 : Receiver.

Problem :

After receiption of frames to node 2 the message buffer indexes configured in register FR_MBIDXRn[MBIDX] for RX frames are getting changed. Because of this received data is written to different message buffer indexes.

Implementation :

I have configured Tx and Rx message buffers when the POC is in CONFIG state and allocated message buffer indexes to each Tx and Rx frames. Refer below image.

pastedImage_3.png

But after frame reception the message buffer indexes of Rx frames are getting changed and due to this received frame data is written to different message buffer indexes. Here I have attached images for your reference which shows data is written to different indexes and FR_MBIDXRn[MBIDX] register values are changed.

Let me know your suggestions to overcome from changing message buffer index or how to handle such scenarios.

Labels (1)
0 Kudos
Reply
1 Reply

1,600 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

The MB receive the data based on the slot number. The changing the MB index is normal functionality of the FlexRay module – see chapter 5 Receiving Frame in the FlexRay document you aleary got.

 

BR, Petr

0 Kudos
Reply