Flash Calibration and Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Calibration and Boot

ソリューションへジャンプ
1,941件の閲覧回数
20Sidar04
Contributor III

Dear Mr./Mrs.

When I viewed datasheet, I saw that boot and calibration example using on Flash Large Block for MPC5777C. What is purpose of boot and calibration on this flash adress?

Best Regards.

 

Flash question.jpgFlash question.jpg

 

タグ(3)
0 件の賞賛
返信
1 解決策
1,931件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is certain use case, these blocks are not somehow special. These are just flash large block.

It is the same as blocks marked as EEPROM - these are also not EEPROM block but small flash blocks somehow suitable for EEPROM emulation.

On these device, MMU is used for remapping of address space, for calibration feature. It can be done also with other block, not only specifically with four mentioned.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,932件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is certain use case, these blocks are not somehow special. These are just flash large block.

It is the same as blocks marked as EEPROM - these are also not EEPROM block but small flash blocks somehow suitable for EEPROM emulation.

On these device, MMU is used for remapping of address space, for calibration feature. It can be done also with other block, not only specifically with four mentioned.

0 件の賞賛
返信