First Feed dog error make a reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

First Feed dog error make a reset

2,792 Views
liujinhang
Contributor III

hi,

we met a problem when we operation the 33907. the problem is the 5744 will not be reset by 33907 when the first feed dog command is error in 256ms initial time window.

in order to be easy to analyze the problem, i made a smallest project to reproduction the fault phenomenon. see the attachment.

Original Attachment has been moved to: MPC5744P_MC33907_8_Demo.zip

Labels (1)
0 Kudos
Reply
5 Replies

2,469 Views
liujinhang
Contributor III

anybody help us?

0 Kudos
Reply

2,469 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Liu,

I suspect that the MC33907 is in the Debug mode. This is why RSTB is not asserted by wrong WD refresh during the INIT phase.

Best regards,

Tomas

0 Kudos
Reply

2,469 Views
liujinhang
Contributor III

Hi tomas ,

have you test the error project?  

if you also find the error as we described, we want to know the reason.

if you cann't find the error, we will find if our project  wrong.

we need to close this problem , please help us. 

0 Kudos
Reply

2,469 Views
liujinhang
Contributor III

hi Tomas,

can you please test the error program just once, to check if we have the problem actually?

thank you very much.

0 Kudos
Reply

2,469 Views
chshli
Contributor II

Hi Tomas,

I'm sure the 33907 is not in the Debug mode.And if the watchdog is not refreshed during this 256 ms open window (INIT FS phase), the device asserts the reset low.

0 Kudos
Reply