FIT Exception Issue MPC5777c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FIT Exception Issue MPC5777c

620 Views
Pavan_Moody
Contributor II

Hi Team, 

 

I am trying produce FIT exception.

        asm("li r0, 0x8000");
        asm("mtspr TCR, r0");
        asm("mtspr TCR, r0");
 

However, after executing this code, the board resets then enters the FIT exception handler. Could you please let me know if any additional configuration or changes are required to correctly trigger and handle the FIT exception?

Thank you for your support.

Best regards,
Pavan

0 Kudos
Reply
7 Replies

588 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The FIT exception should work once the exception infrastructure is properly configured.

Please verify:

  • IVPR points to a valid exception vector table.
  • IVOR10 is configured for the FIT handler.
  • Interrupts are enabled (MSR[EE] = 1).
  • The time base/FIT source is running.

Since the board resets before reaching the FIT handler, please also check the RGM reset status registers to identify the reset source.

Reference: FIT exception generation is described in AN2865 Section 3.

Best regards,
Peter

0 Kudos
Reply

541 Views
Pavan_Moody
Contributor II
Hello,

MTSPR(SPR_HID0, 16#00004000#); -- Enable TB status
MTSPR(SPR_TCR, 16#04800000#); -- Enable DEC +FIT
MTSPR(SPR_TSR, 16#04000000#);
i think is this correct iam enabling properly
0 Kudos
Reply

539 Views
Pavan_Moody
Contributor II
MTSPR(SPR_HID0, 16#00004000#); -- Enable TB
MTSPR(SPR_TCR, 16#001814000#); -- EnableDEC+FIT
MTSPR(SPR_TSR, 16#004000000#);
Here iam following up This document https://www.nxp.com/docs/en/application-note/AN2865.pdf
0 Kudos
Reply

583 Views
Pavan_Moody
Contributor II
Hi,

IVPR points to a valid exception vector table
yes.

IVOR10 is configured for the FIT handler.
No. configured to IVOR11.

Interrupts are enabled (MSR[EE] = 1).
yes. BSP_MSR_Normal: Unsigned_32 :=16#02009000#;

The time base/FIT source is running.
yes.

You can find the details. which i configured help me out anything else i need to do

Regards,
Pavan
0 Kudos
Reply

547 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Thank you for the update. Since you are using FIT, IVOR11 is the correct vector. Please additionally verify:

  • TCR[FIE] = 1 (FIT interrupt enabled)
  • FIT period selection (TCR[FP])
  • TSR[FIS] becomes set when the FIT interval expires
  • The FIT handler clears TSR[FIS]
  • IVOR11 entry in the exception table contains the correct branch to the FIT ISR
  • RGM reset status registers to determine whether another exception or reset occurs before entering the FIT handler

The value of TSR is particularly important. If TSR[FIS] is set but the ISR is not entered, the FIT is being generated but the exception dispatch path is not functioning correctly.

Best regards,

Peter

0 Kudos
Reply

585 Views
Pavan_Moody
Contributor II
Hi

MTSPR(IVOR10, entDECR'Address); -- Decrementer (handled by Ada runtime)
-- Now use e200/MPC55xx mapping
MTSPR(IVOR11, ent0B'Address); -- Fixed Interval Timer.. This will work by making IVOR10 as FIT.

Regards,
Pavan
0 Kudos
Reply

606 Views
sulaxna068debi
Contributor I

Hello, 

I’d first check that the FIT enable bit in the TCR is set correctly and that the corresponding exception vector is properly initialized. Also make sure the exception/MSR configuration allows the FIT interrupt to be taken.

One thing that stands out is writing the same value to TCR twice:

asm("li r0, 0x8000");
asm("mtspr TCR, r0");
asm("mtspr TCR, r0");

If your intention is simply to force the FIT event, you may not need the second write. The exact behavior also depends on the PowerPC core and the TCR bit definitions for that specific device. 

0 Kudos
Reply