FCCU problems about MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FCCU problems about MPC5744P

2,531 Views
qm1013
Contributor III

hello, I have some problems, about the FCCU .

The example is provided by NXP (MPC574xP Quick Start Package Rev10).

TIM截图20200511170722.jpg

I have change the setting of the FCCU, to test the sequence of the EOUT[0] and EOUT[1]. Bellow is the setting .

TIM截图20200511171346.jpg

When the FOM of the FCCU_CFG regisger is set to 0b010 (Bistable) . The output is not change when FCCU go to error state. The sequence of the EOUT[0] and EOUT[1] is not right. EOUT[0] is always high, and EOUT[1] is always low.

They do  not change when the FCCU state changes.

But when the FOM of the FCCU_CFG register is set to 0b000(Dual-Rail) or 0b001(Time-Switching). The output sequence of the EOUT[0] and EOUT[1]  is right.

Could you give me some advices about the setting of the FCCU ? Is there a mistake in the configuration?

regards,

meng

0 Kudos
Reply
2 Replies

2,485 Views
qm1013
Contributor III

I make some mistakes,I have solved the problem. Thank you very much.

regards,

meng

0 Kudos
Reply

1,844 Views
shaoduoduo
Contributor I

I have encountered the same problem as you. How did you solve it?!!!!

 

FYI

0 Kudos
Reply