External interrupt MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External interrupt MPC5748G

1,185件の閲覧回数
Mustafa123
Contributor I

Hallo and Good afternoon,

 

please i try to use  External interrupt PA3 on MPC5748G but until now not work  please if any one has experience with this problem i will be thankful

 

Code:

int main(void) {

xcptn_xmpl(); /* Configure and Enable Interrupts */
peri_clock_gating();
SIUL2.MSCR[10].B.OBE = 1;

extern_interrupt();

for (;;) {

}

}

void extern_interrupt(void) {
// INTC.PSR[1].B.PRC_SELN1 = 0x4; /* IRQ sent to Core 1 */
// INTC.PSR[1].B.PRIN = 0x0F; /* IRQ priority = 4 (15 = highest) */


SIUL2.IRER0.B.EIRE0 = 1; // CLEAR the flag
SIUL2.IRSR0.B.DIRSR0= 0; // request Enabel
SIUL2.IFEER0.B.IFEE0 = 1;   
SIUL2.MSCR[3].B.OBE = 0; // output pin disable
SIUL2.MSCR[3].B.IBE = 1; // input pin enabel
SIUL2.IMCR[144].B.SSS=1;   // depend on the datasheet excel
SIUL2.IRER0.B.EIRE0 = 0; // Enabel interrupt flag in 1
}

void extern_ISR(void) {
uint16_t i, j;
for (i = 0; i < 15000; i++)
SIUL2.GPDO[10].R = 1;
for (j = 0; j < 15000; j++)
SIUL2.GPDO[10].R = 0;

SIUL2.IRER0.B.EIRE0 = 1; // disable the flag
}

 

IRQ.C

void dummy (void);

extern void extern_ISR(void);

(uint32_t) &extern_ISR, /* Vector # 243 SIUL EIRQ [0-7] - SIUL Combined External Interrupt */
(uint32_t) &dummy, /* Vector # 244 SIUL EIRQ [8-15] - SIUL Combined External Interrupt */
(uint32_t) &dummy, /* Vector # 245 SIUL EIRQ [16-23] - SIUL Combined External Interrupt */
(uint32_t) &dummy, /* Vector # 246 SIUL EIRQ [24-31] - SIUL Combined External Interrupt */

Thank you very much 

0 件の賞賛
返信
1 返信

1,147件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Interrupt flag is needed to clear by write to SIUL2_ISR0 register. not to SIUL2_IRER0.

I could possibly point out following thread:
https://community.nxp.com/t5/MPC5xxx/External-Interrupt-MPC5748g-is-not-working-what-do-I-miss/m-p/7...

Also I would recommend to see following bulleting to understand when use .B and when .R instance:
https://www.nxp.com/docs/en/engineering-bulletin/EB758.pdf

 

0 件の賞賛
返信