Examples or tutorials for using SDHC in MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Examples or tutorials for using SDHC in MPC5748G

2,979件の閲覧回数
jlee4
Contributor II

Hi,

I am trying to insert a micro SD card in the corresponding SDHC port of MPC5748G and use it for saving and loading file. Since I am quite new about embedded system, could you introduce me a good examples or tutorials about how to use SDHC? (I understand the communication between the board and the SD card is done by SPI communication and the port numbers are provided in the pinmap (https://www.nxp.com/docs/en/quick-reference-guide/DEVKIT-MPC5748G-QSG.pdf), but I have no idea what to do for further progress.)

 

Best,

Jongwon

0 件の賞賛
返信
4 返答(返信)

2,956件の閲覧回数
jlee4
Contributor II

Ah, I am a Linux user, and it seems like there is no SDHC example on the Linux version of S32DS. Could you provide me any resources also available in S32DS for Linux? (Just sharing the example file will be also welcomed!)

0 件の賞賛
返信

2,973件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

SW examples can be found in S32 Design Studio IDE:

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

The examples can be found in this folder:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\

Regards,

Lukas

 

0 件の賞賛
返信

2,950件の閲覧回数
jlee4
Contributor II

Ah, I am a Linux user, and it seems like there is no SDHC example on the Linux version of S32DS. Could you provide me any resources also available in S32DS for Linux? (Just sharing the example file will be also welcomed!)

0 件の賞賛
返信

2,945件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I have bad news... The SDK is integrated only in Windows version:

lukaszadrapa_0-1605271915473.pnglukaszadrapa_0-1605271915473.png

Unfortunately we do not have other examples than this one in SDK.

Regards,

Lukas

 

0 件の賞賛
返信