Example code for context switch for MPC56XX PowerPC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example code for context switch for MPC56XX PowerPC

ソリューションへジャンプ
3,733件の閲覧回数
alonsovallejo
Contributor I

Hello All,

I am working into a project with automotive microncontroller MPC5604B. I have all the software of a scheduler preentive base and I based in Handler_ISR to know how to the context switch, but i dont know how to perform the context swich or which other handlers I need to use. Is there any example code about how to do this becuase EABI is not completly clear,

thanks.

1 解決策
3,441件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Dear Alonso Vallejo, 

Your
requirement is very similar to context switching which is done when interrupt
handler is executed, you can also use the same sequence.

 

Saving context:
    stwu    r1, -0x50 (r1)    /* Create stack frame */
    stw r0,  0x24 (r1)        /* Store r0 working register  */

    /* Save SRR0 and SRR1 */
    mfsrr1  r0                /* Store SRR1 (must be done before enabling EE) */
    stw     r0,  0x10 (r1)
    mfsrr0  r0                /* Store SRR0 (must be done before enabling EE) */
    stw     r0,  0x0C (r1)

    /* Clear request to processor; r3 contains the address of the ISR */
    stw     r3,  0x28 (r1)    /* Store r3 */
    lis     r3, INTC_IACKR@h  /* Read pointer into ISR Vector Table & store in r3     */
    ori     r3, r3, INTC_IACKR@l
    lwz     r3, 0x0(r3)       /* Load INTC_IACKR, which clears request to processor   */
    lwz     r3, 0x0(r3)       /* Read ISR address from ISR Vector Table using pointer */

    /* Enable processor recognition of interrupts */
    wrteei  1                   /* Set MSR[EE]=1  */

    /* Save rest of context required by EABI */
    stw     r12, 0x4C (r1)      /* Store r12 */
    stw     r11, 0x48 (r1)      /* Store r11 */
    stw     r10, 0x44 (r1)      /* Store r10 */
    stw     r9,  0x40 (r1)      /* Store r9 */
    stw     r8,  0x3C (r1)      /* Store r8 */
    stw     r7,  0x38 (r1)      /* Store r7 */
    stw     r6,  0x34 (r1)      /* Store r6 */
    stw     r5,  0x30 (r1)      /* Store r5 */
    stw     r4,  0x2C (r1)      /* Store r4 */
    mfcr    r0                  /* Store CR */
    stw     r0,  0x20 (r1)
    mfxer   r0                  /* Store XER */
    stw     r0,  0x1C (r1)
    mfctr   r0                  /* Store CTR */
    stw     r0,  0x18 (r1)
    mflr    r0                  /* Store LR */
    stw     r0,  0x14 (r1)

 

Restoring context:
    /* Restore context required by EABI (except working registers) */
    lwz     r0,  0x14 (r1)      /* Restore LR */
    mtlr    r0
    lwz     r0,  0x18 (r1)      /* Restore CTR */
    mtctr   r0
    lwz     r0,  0x1C (r1)      /* Restore XER */
    mtxer   r0
    lwz     r0,  0x20 (r1)      /* Restore CR */
    mtcrf   0xff, r0
    lwz     r5,  0x30 (r1)      /* Restore r5 */
    lwz     r6,  0x34 (r1)      /* Restore r6 */
    lwz     r7,  0x38 (r1)      /* Restore r7 */
    lwz     r8,  0x3C (r1)      /* Restore r8 */
    lwz     r9,  0x40 (r1)      /* Restore r9 */
    lwz     r10, 0x44 (r1)      /* Restore r10 */
    lwz     r11, 0x48 (r1)      /* Restore r11 */
    lwz     r12, 0x4C (r1)      /* Restore r12 */

    /* Disable processor recognition of interrupts */
    wrteei  0

    /* Ensure interrupt flag has finished clearing */
    mbar    0

    /* Write 0 to INTC_EOIR, informing INTC to lower priority */
    li      r3, 0
    lis     r4, INTC_EOIR@h     /* Load upper half of INTC_EOIR address to r4 */
    ori     r4, r4, INTC_EOIR@l
    stw     r3, 0(r4)           /* Write 0 to INTC_EOIR */

    /* Restore Working Registers */
    lwz     r3,  0x28 (r1)      /* Restore r3 */
    lwz     r4,  0x2C (r1)      /* Restore r4 */

    /* Retrieve SRR0 and SRR1 */
    lwz     r0,  0x0C (r1)      /* Restore SRR0 */
    mtsrr0  r0
    lwz     r0,  0x10 (r1)      /* Restore SRR1 */
    mtsrr1  r0

    /* Restore Other Working Registers */
    lwz     r0,  0x24 (r1)      /* Restore r0 */

    /* Restore space on stack */
    addi    r1, r1, 0x50

  
Please remember, this is only example code which can need some changes in your project, but from my point of view, this is good base for your development.

Regards,

Martin

元の投稿で解決策を見る

2 返答(返信)
3,441件の閲覧回数
zhouxian
Contributor III

How to save and restore floating point unit registers? Thanks!

0 件の賞賛
返信
3,442件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Dear Alonso Vallejo, 

Your
requirement is very similar to context switching which is done when interrupt
handler is executed, you can also use the same sequence.

 

Saving context:
    stwu    r1, -0x50 (r1)    /* Create stack frame */
    stw r0,  0x24 (r1)        /* Store r0 working register  */

    /* Save SRR0 and SRR1 */
    mfsrr1  r0                /* Store SRR1 (must be done before enabling EE) */
    stw     r0,  0x10 (r1)
    mfsrr0  r0                /* Store SRR0 (must be done before enabling EE) */
    stw     r0,  0x0C (r1)

    /* Clear request to processor; r3 contains the address of the ISR */
    stw     r3,  0x28 (r1)    /* Store r3 */
    lis     r3, INTC_IACKR@h  /* Read pointer into ISR Vector Table & store in r3     */
    ori     r3, r3, INTC_IACKR@l
    lwz     r3, 0x0(r3)       /* Load INTC_IACKR, which clears request to processor   */
    lwz     r3, 0x0(r3)       /* Read ISR address from ISR Vector Table using pointer */

    /* Enable processor recognition of interrupts */
    wrteei  1                   /* Set MSR[EE]=1  */

    /* Save rest of context required by EABI */
    stw     r12, 0x4C (r1)      /* Store r12 */
    stw     r11, 0x48 (r1)      /* Store r11 */
    stw     r10, 0x44 (r1)      /* Store r10 */
    stw     r9,  0x40 (r1)      /* Store r9 */
    stw     r8,  0x3C (r1)      /* Store r8 */
    stw     r7,  0x38 (r1)      /* Store r7 */
    stw     r6,  0x34 (r1)      /* Store r6 */
    stw     r5,  0x30 (r1)      /* Store r5 */
    stw     r4,  0x2C (r1)      /* Store r4 */
    mfcr    r0                  /* Store CR */
    stw     r0,  0x20 (r1)
    mfxer   r0                  /* Store XER */
    stw     r0,  0x1C (r1)
    mfctr   r0                  /* Store CTR */
    stw     r0,  0x18 (r1)
    mflr    r0                  /* Store LR */
    stw     r0,  0x14 (r1)

 

Restoring context:
    /* Restore context required by EABI (except working registers) */
    lwz     r0,  0x14 (r1)      /* Restore LR */
    mtlr    r0
    lwz     r0,  0x18 (r1)      /* Restore CTR */
    mtctr   r0
    lwz     r0,  0x1C (r1)      /* Restore XER */
    mtxer   r0
    lwz     r0,  0x20 (r1)      /* Restore CR */
    mtcrf   0xff, r0
    lwz     r5,  0x30 (r1)      /* Restore r5 */
    lwz     r6,  0x34 (r1)      /* Restore r6 */
    lwz     r7,  0x38 (r1)      /* Restore r7 */
    lwz     r8,  0x3C (r1)      /* Restore r8 */
    lwz     r9,  0x40 (r1)      /* Restore r9 */
    lwz     r10, 0x44 (r1)      /* Restore r10 */
    lwz     r11, 0x48 (r1)      /* Restore r11 */
    lwz     r12, 0x4C (r1)      /* Restore r12 */

    /* Disable processor recognition of interrupts */
    wrteei  0

    /* Ensure interrupt flag has finished clearing */
    mbar    0

    /* Write 0 to INTC_EOIR, informing INTC to lower priority */
    li      r3, 0
    lis     r4, INTC_EOIR@h     /* Load upper half of INTC_EOIR address to r4 */
    ori     r4, r4, INTC_EOIR@l
    stw     r3, 0(r4)           /* Write 0 to INTC_EOIR */

    /* Restore Working Registers */
    lwz     r3,  0x28 (r1)      /* Restore r3 */
    lwz     r4,  0x2C (r1)      /* Restore r4 */

    /* Retrieve SRR0 and SRR1 */
    lwz     r0,  0x0C (r1)      /* Restore SRR0 */
    mtsrr0  r0
    lwz     r0,  0x10 (r1)      /* Restore SRR1 */
    mtsrr1  r0

    /* Restore Other Working Registers */
    lwz     r0,  0x24 (r1)      /* Restore r0 */

    /* Restore space on stack */
    addi    r1, r1, 0x50

  
Please remember, this is only example code which can need some changes in your project, but from my point of view, this is good base for your development.

Regards,

Martin