Example_MPC5748G_FlexCAN_FD_TX_RX_test_S32DS_21 usage question?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example_MPC5748G_FlexCAN_FD_TX_RX_test_S32DS_21 usage question?

604件の閲覧回数
xiha
Contributor II

My project referred to the routine of the website.(Example_MPC5748G_FlexCAN_FD_TX_RX_test_S32DS_21 )

When I use this exmple provided by the website to send data, flexcan has access to the data I send???why I can get the data that I send.

/* enable the FlexCAN module, reset and freeze */
CAN_0.MCR.R = (0
| FLEXCAN_MCR_FRZ /* enabled to enter Freeze mode */
| FLEXCAN_MCR_HALT /* enter freeze mode if FRZ bit is set */
//| FLEXCAN_MCR_SOFTRST /* soft reset */
//| FLEXCAN_MCR_SRXDIS /* self reception enabled */
| FLEXCAN_MCR_BCC /* individual Rx masking and queue */
| 0x00000003);

 

/*******************************************************************************
Function Name : TransmitMsgFD
Engineer      : Petr Stancik
Date          : Jun-22-2021
Parameters    : mb ... mb number used
                ext ... 0-standard ID, 1-extended ID
                ID ... ID to be sent
                length ... number of bytes to be sent
Modifies      : NONE
Returns       : NONE
Notes         : Transmit message once using selected MB
Issues        : NONE
*******************************************************************************/
void TransmitMsgFD(uint32_t mb, uint8_t ext, uint32_t ID, uint8_t length)
{
/* Assumption:  Message buffer CODE is INACTIVE */
  uint8_t   i,dlc,z=0;
  uint32_t *pTxMB = GetMBAddr(mb);
  uint32_t txID = (ext==0) ? ID<<18 : ID;

  /*calculate dlc value from no. bytes*/
  if(length < 0x09)
  {
      dlc = length;
  }else if(length < 0x0D){
      dlc = 0x9;
  }else if(length < 0x11){
      dlc = 0xA;
  }else if(length < 0x15){
      dlc = 0xB;
  }else if(length < 0x19){
      dlc = 0xC;
  }else if(length < 0x21){
      dlc = 0xD;
  }else if(length < 0x31){
      dlc = 0xE;
  }else{
      dlc = 0xF;
  }


  *(pTxMB + 1) = txID;  // write ID

  for (i=0; i<length/4; i++,z+=4) {
    *(pTxMB + 2 + i) =  z<<24 | (z+1)<<16 | (z+2)<< 8 | z+3;      /* Data to be transmitted */
  }

  *pTxMB = (0   // Tx Buffer 0 T0 word
           | 1<<31  // extended Data Length
           | 1<<30  // bit rate switch
           | 0xC<<24    // code = 0xC, TX once
           | 1<<22  // SRR = 1
           | ext<<21    // IDE
           | 0<<20  // RTR = 0
           | dlc<<16);  // DLC

  while (!(CAN_0.IFLAG1.R & 1<<mb)) {};  /* Wait for CAN 0 MB 0 flag */
  CAN_0.IFLAG1.R = 1<<mb;   // clear MB flag
}
 
/*******************************************************************************
Function Name : ReceiveMsgFD
Engineer      : Petr Stancik
Date          : Jun-22-2021
Parameters    : mb ... MB number used
Modifies      : NONE
Returns       : NONE
Notes         : check if given MB have new message, if yes, read it
Issues        : NONE
*******************************************************************************/
void ReceiveMsgFD(uint32_t mb)
{
  uint8_t j;
  uint32_t dummy,dlc;
  uint32_t *pRxMB = GetMBAddr(mb);
  uint8_t *pRxMBdata = (uint8_t *)(&pRxMB[2]);

  if(CAN_0.IFLAG1.R & 1<<mb)  // if CAN 0 MB flag set
  {
        /* Read CODE, ID, LENGTH, DATA, TIMESTAMP*/
        dummy = *pRxMB;
        RxCODE   = (dummy>>24) & 0xF;
        RxID     = *(pRxMB+1);
        dlc = (dummy>>16) & 0xF;

        /*calculate no. bytes from dlc value*/
        if(dlc < 0x09)
        {
            RxLENGTH = dlc;
        }else if(dlc == 0x9){
            RxLENGTH = 12;
        }else if(dlc == 0xA){
            RxLENGTH = 16;
        }else if(dlc == 0xB){
            RxLENGTH = 20;
        }else if(dlc == 0xC){
            RxLENGTH = 24;
        }else if(dlc == 0xD){
            RxLENGTH = 32;
        }else if(dlc == 0xE){
            RxLENGTH = 48;
        }else{
            RxLENGTH = 64;
        }

        for (j=0; j<RxLENGTH; j++) {
          RxDATA[j] = *pRxMBdata++ ;
        }
        RxTIMESTAMP = dummy & 0xFF;;
        dummy = CAN_0.TIMER.R;      // Read TIMER to unlock message buffers
        CAN_0.IFLAG1.R = 1<<mb;     // clear MB flag
  }

}
0 件の賞賛
返信
0 返答(返信)