Error during Debug in MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error during Debug in MPC5777C

2,672 次查看
sourabhjain
Contributor III

Hi i am trying to debug a code in MPC5777C so during debug the code stuck at particular line and showing an error like this

Program received signal SIGINT, Interrupt.
0x00c10010 in IVOR1_Vector ()
No source available for "IVOR1_Vector() at 0xc10010"

but when i comment the line where code stuck then the code debug properly and generate result 

so can you please find what is this error for and why my code stuck ?

标签 (1)
4 回复数

2,409 次查看
petervlna
NXP TechSupport
NXP TechSupport

First of all focus on what is the source of IVOR1. (Critical or NMI interrupt?)

Do you have programed IVOR1 handler?

When you step assembly in the code do you see correct instruction execution?

Peter

2,409 次查看
sourabhjain
Contributor III

Processor : MPC5777C

Debugger : Multilink Universal Fx

void my_system_etpu_init(void)
{
int32_t error_code;
int V_duty=0;
int C1_TOP_duty=0;

alpha_delay= ((float)(alpha_initial))*10.0/180;

fs_etpu_init( my_etpu_config, (uint32_t *)etpu_code, sizeof(etpu_code), \
(uint32_t *)etpu_globals, sizeof(etpu_globals));


/*** LV to HV side ***/

error_code = fs_etpu_spwm_init_master ( ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP),
300000, //freq
10, //duty
FS_ETPU_TCR2, //timebase
etpu_a_tcr2_freq, //timebase_freq
FS_ETPU_SPWM_IMMEDIATE, //ref mode
0, //ref ptr ; has no meaning im immediate mode
FS_ETPU_SPWM_FALLING_EDGE_INT_DMA,
0x04000004, //link1
0x04000004
);
Master2_rising_edge_ptr = fs_etpu_data_ram(ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP)) +
(uint32_t) ((uint32_t *) (FS_ETPU_SPWM_RISING_OFFSET >>2)) -
(uint32_t) ((uint32_t *) ((fs_etpu_data_ram_start) / 4)) ;


Master2_rising_edge_ptr8 = (uint8_t *)Master2_rising_edge_ptr + 1 ;
Master2_rising_edge_ptr = (uint32_t *)Master2_rising_edge_ptr8 ;

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_C1_BOT),
FS_ETPU_PRIORITY_MIDDLE,
300000, //freq
10, // 25% duty
1.6, // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master2_rising_edge_ptr
);


error_code = fs_etpu_spwm_init_master ( ETPU_ENGINE_A_CHANNEL(PWM_A1_TOP),
50000,// freq
1, // duty
FS_ETPU_TCR2,// timebase
etpu_a_tcr1_freq, //timebase_freq
FS_ETPU_SPWM_IMMEDIATE, //ref mode
0, //ref ptr has no meaning im immediate mode
FS_ETPU_SPWM_FALLING_EDGE_INT_DMA,
0x02000302, //link1
0x81828083
);

Master1_rising_edge_ptr = fs_etpu_data_ram(ETPU_ENGINE_A_CHANNEL(PWM_A1_TOP)) +
(uint32_t) ((uint32_t *) (FS_ETPU_SPWM_RISING_OFFSET >>2)) -
(uint32_t) ((uint32_t *) ((fs_etpu_data_ram_start) / 4)) ;


Master1_rising_edge_ptr8 = (uint8_t *)Master1_rising_edge_ptr + 1 ;
Master1_rising_edge_ptr = (uint32_t *)Master1_rising_edge_ptr8 ;

///**HV to LV side *


error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_B1_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
1, // 25% duty
alpha_delay, // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_A1_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
10, // 25% duty
(TDC + DEADTIME), // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);
error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_B1_TOP),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
1, // 25% duty
TDC+ DEADTIME+ alpha_delay, // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_B_CHANNEL(PWM_A2_TOP),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
0, //10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_B_CHANNEL(PWM_B2_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
alpha_delay, //10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_B_CHANNEL(PWM_A2_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
(TDC + DEADTIME), //20 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave (ETPU_ENGINE_B_CHANNEL(PWM_B2_TOP),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
(TDC + DEADTIME)+alpha_delay, //10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);
my_system_etpu_start();

fs_etpu_spwm_run_master (ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP),
FS_ETPU_PRIORITY_MIDDLE);

fs_etpu_spwm_run_master (ETPU_ENGINE_A_CHANNEL(PWM_A1_TOP),
FS_ETPU_PRIORITY_MIDDLE);


for(C1_TOP_duty=11;C1_TOP_duty<41;C1_TOP_duty++)
{
fs_etpu_spwm_duty(ETPU_ENGINE_A_CHANNEL(PWM_C1_BOT),C1_TOP_duty*100);
fs_etpu_spwm_duty(ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP),C1_TOP_duty*100);

}

}

here is my code at the end where i try to update duty cycle from 11% to 40% in this the line which is bold type where my code stuck and when i stop the debug then this type of error come given below.

Program received signal SIGINT, Interrupt.
0x00c10010 in IVOR1_Vector ()
No source available for "IVOR1_Vector() at 0xc10010"

if i comment the line in bold then the loop run fine and code execute successfully.

i also try to update etpu_set.h written below where i comment the additional zero which are shown here in bold letter because of this some times code run and sometimes do not.

const uint32_t etpu_code[] = { 0xC088C088,0xC088C088,0x00340023,0x005A005A,
0x0082406C,0x40864041,0x0082406C,0x40864041,
0x407C0082,0x40534086,0x407C0082,0x40534086,
0x407C406C,0x40534041,0x407C406C,0x40534041,
0xF320027F,0x3BF93FB4,0x0003301D,0xF28002BF,
0x00033099,0xF2C002FF,0x00033119,0xF200033F,
0x00033219,0xF240037F,0x00033819,0x9FF37A00,
0xFFFFCCF9,0x4FEFF6BF,0x3BF01FD4,0x3BF11FD4,
0x3BF71FD4,0xFFFFCCF9,0x3BF21FD4,0x4FF8FDFE,
0xFFFBFCF9,0xCFE9FE82,0xFFEFFAD9,0xBFE80A80,
0xBF092A80,0xBFFFFB8A,0xBFEFFB81,0x3B1E3FF4,
0xBFF37A89,0xFB3F0CFB,0xCFEFF884,0xFFC003DF,
0xCFEFF885,0xFFC003DF,0xBFFE7A86,0xF7C0071F,
0x4FF8FDFE,0xFFFAFCF9,0xCFF9FD01,0x7FFFFFFD,
0xF3A0077F,0x580006A5,0x4FF33FFF,0x495FFFFF,
0xBFEFFB81,0x3BF8FFF4,0xF0C0081F,0x4AFFFFFF,
0x6FFFFFFF,0xCFE8FA8A,0x3B1E2FF4,0x49FFFFFF,
0xBFEFFB81,0x3BF8FFF4,0xF0C0091F,0x4AFFFFFF,
0xBFFE7A86,0xDFEF3A81,0xBF1E7A89,0xBFEFFB80,
0xBFFFFB8A,0xCFEFF884,0xFFC003DF,0xCFEFF885,
0xFFC003DF,0xFFFF3CF9,0xF7FF7CF9,0xBFEFFB89,
0x3BF83FF4,0xF3E00B3F,0xFFF9CCFB,0xFFFF3CF9,
0xFFFF7CF9,0x6FFFFFFF,0xCFEFF981,0x3BF20BF4,
0xF0C00CFF,0x3DFFAFF4,0xCFFFF981,0xBFEFFF87,
0xFFEFFAD9,0xBFE80A83,0xBF092A81,0xBFFFFB8B,
0x7F1E3F59,0xF7E00D7F,0xFF3F5CFB,0xBFEFFF87,
0xFFEFFAD9,0xBFE80A83,0xBF197A86,0x47FFF7FF,
0xF3000DDF,0xF7C00CFF,0xBFEFFB86,0x3BF82FF4,
0xFFF83CFB,0x49FFFFFF,0xBFEFFB8B,0x3BF8FFF4,
0xF0C00EDF,0x4AFFFFFF,0xBFEFFB86,0xBFE80A8B,
0xBF197A89,0xBFEFFB81,0xBFFFFB8B,0x6FFFFFFF,
0xF3000FDF,0xF7C00CFF,0xBFEFFB89,0x3BF83FF4,
0xFFF9CCFB,0x6FFFFFFF,0xF300109F,0xF7C00CFF,
0xFFC0021F,0x6FFFFFFF,0xFFC0021F,0x6FFFFFFF,
0x6FFFFFFF,0x00000000,0x00000000,0x00000000
#if 0
,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000

#endif

}

0 项奖励
回复

2,409 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I am afraid that we need more details if you want us to help you.

Compiler? Debugger?

Is this your code? etc..

If you step it in debugger assembly do you see proper instruction execution? Are you core registers loaded correctly?

Give us more details then just your failing line.

Peter

2,409 次查看
sourabhjain
Contributor III

Processor : MPC5777C

Debugger : Multilink Universal Fx

below is the code which i am using for debug

void my_system_etpu_init(void)
{
int32_t error_code;
int V_duty=0;
int C1_TOP_duty=0;

alpha_delay= ((float)(alpha_initial))*10.0/180;

fs_etpu_init( my_etpu_config, (uint32_t *)etpu_code, sizeof(etpu_code), \
(uint32_t *)etpu_globals, sizeof(etpu_globals));


/*** LV to HV side ***/

error_code = fs_etpu_spwm_init_master ( ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP),
300000, //freq
10, //duty
FS_ETPU_TCR2, //timebase
etpu_a_tcr2_freq, //timebase_freq
FS_ETPU_SPWM_IMMEDIATE, //ref mode
0, //ref ptr ; has no meaning im immediate mode
FS_ETPU_SPWM_FALLING_EDGE_INT_DMA,
0x04000004, //link1
0x04000004
);
Master2_rising_edge_ptr = fs_etpu_data_ram(ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP)) +
(uint32_t) ((uint32_t *) (FS_ETPU_SPWM_RISING_OFFSET >>2)) -
(uint32_t) ((uint32_t *) ((fs_etpu_data_ram_start) / 4)) ;


Master2_rising_edge_ptr8 = (uint8_t *)Master2_rising_edge_ptr + 1 ;
Master2_rising_edge_ptr = (uint32_t *)Master2_rising_edge_ptr8 ;

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_C1_BOT),
FS_ETPU_PRIORITY_MIDDLE,
300000, //freq
10, // 25% duty
1.6, // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master2_rising_edge_ptr
);


error_code = fs_etpu_spwm_init_master ( ETPU_ENGINE_A_CHANNEL(PWM_A1_TOP),
50000,// freq
1, // duty
FS_ETPU_TCR2,// timebase
etpu_a_tcr1_freq, //timebase_freq
FS_ETPU_SPWM_IMMEDIATE, //ref mode
0, //ref ptr has no meaning im immediate mode
FS_ETPU_SPWM_FALLING_EDGE_INT_DMA,
0x02000302, //link1
0x81828083
);

Master1_rising_edge_ptr = fs_etpu_data_ram(ETPU_ENGINE_A_CHANNEL(PWM_A1_TOP)) +
(uint32_t) ((uint32_t *) (FS_ETPU_SPWM_RISING_OFFSET >>2)) -
(uint32_t) ((uint32_t *) ((fs_etpu_data_ram_start) / 4)) ;


Master1_rising_edge_ptr8 = (uint8_t *)Master1_rising_edge_ptr + 1 ;
Master1_rising_edge_ptr = (uint32_t *)Master1_rising_edge_ptr8 ;

 

 

///**HV to LV side *


error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_B1_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
1, // 25% duty
alpha_delay, // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_A1_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
10, // 25% duty
(TDC + DEADTIME), // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);
error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_A_CHANNEL(PWM_B1_TOP),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
1, // 25% duty
TDC+ DEADTIME+ alpha_delay, // 10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_B_CHANNEL(PWM_A2_TOP),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
0, //10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_B_CHANNEL(PWM_B2_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
alpha_delay, //10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave ( ETPU_ENGINE_B_CHANNEL(PWM_A2_BOT),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
(TDC + DEADTIME), //20 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);

error_code = fs_etpu_spwm_init_slave (ETPU_ENGINE_B_CHANNEL(PWM_B2_TOP),
FS_ETPU_PRIORITY_MIDDLE,
50000, //freq
4000, //25% duty
(TDC + DEADTIME)+alpha_delay, //10 us delay
FS_ETPU_TCR2, // timebase
etpu_a_tcr1_freq,
Master1_rising_edge_ptr
);
my_system_etpu_start();

fs_etpu_spwm_run_master (ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP),
FS_ETPU_PRIORITY_MIDDLE);

fs_etpu_spwm_run_master (ETPU_ENGINE_A_CHANNEL(PWM_A1_TOP),
FS_ETPU_PRIORITY_MIDDLE);


for(C1_TOP_duty=11;C1_TOP_duty<41;C1_TOP_duty++)
{
fs_etpu_spwm_duty(ETPU_ENGINE_A_CHANNEL(PWM_C1_BOT),C1_TOP_duty*100);
fs_etpu_spwm_duty(ETPU_ENGINE_A_CHANNEL(PWM_C1_TOP),C1_TOP_duty*100);

}

}

here is my code at the end where i try to update duty cycle from 11% to 40% in this the line which is bold type where my code stuck and when i stop the debug then this type of error come given below.

 

Program received signal SIGINT, Interrupt.
0x00c10010 in IVOR1_Vector ()
No source available for "IVOR1_Vector() at 0xc10010"

 

 

if i comment the line in bold then the loop run fine and code execute successfully.

 

i also try to update etpu_set.h written below where i comment the additional zero which are shown here in bold letter because of this some times code run and sometimes do not.

 

const uint32_t etpu_code[] = { 0xC088C088,0xC088C088,0x00340023,0x005A005A,
0x0082406C,0x40864041,0x0082406C,0x40864041,
0x407C0082,0x40534086,0x407C0082,0x40534086,
0x407C406C,0x40534041,0x407C406C,0x40534041,
0xF320027F,0x3BF93FB4,0x0003301D,0xF28002BF,
0x00033099,0xF2C002FF,0x00033119,0xF200033F,
0x00033219,0xF240037F,0x00033819,0x9FF37A00,
0xFFFFCCF9,0x4FEFF6BF,0x3BF01FD4,0x3BF11FD4,
0x3BF71FD4,0xFFFFCCF9,0x3BF21FD4,0x4FF8FDFE,
0xFFFBFCF9,0xCFE9FE82,0xFFEFFAD9,0xBFE80A80,
0xBF092A80,0xBFFFFB8A,0xBFEFFB81,0x3B1E3FF4,
0xBFF37A89,0xFB3F0CFB,0xCFEFF884,0xFFC003DF,
0xCFEFF885,0xFFC003DF,0xBFFE7A86,0xF7C0071F,
0x4FF8FDFE,0xFFFAFCF9,0xCFF9FD01,0x7FFFFFFD,
0xF3A0077F,0x580006A5,0x4FF33FFF,0x495FFFFF,
0xBFEFFB81,0x3BF8FFF4,0xF0C0081F,0x4AFFFFFF,
0x6FFFFFFF,0xCFE8FA8A,0x3B1E2FF4,0x49FFFFFF,
0xBFEFFB81,0x3BF8FFF4,0xF0C0091F,0x4AFFFFFF,
0xBFFE7A86,0xDFEF3A81,0xBF1E7A89,0xBFEFFB80,
0xBFFFFB8A,0xCFEFF884,0xFFC003DF,0xCFEFF885,
0xFFC003DF,0xFFFF3CF9,0xF7FF7CF9,0xBFEFFB89,
0x3BF83FF4,0xF3E00B3F,0xFFF9CCFB,0xFFFF3CF9,
0xFFFF7CF9,0x6FFFFFFF,0xCFEFF981,0x3BF20BF4,
0xF0C00CFF,0x3DFFAFF4,0xCFFFF981,0xBFEFFF87,
0xFFEFFAD9,0xBFE80A83,0xBF092A81,0xBFFFFB8B,
0x7F1E3F59,0xF7E00D7F,0xFF3F5CFB,0xBFEFFF87,
0xFFEFFAD9,0xBFE80A83,0xBF197A86,0x47FFF7FF,
0xF3000DDF,0xF7C00CFF,0xBFEFFB86,0x3BF82FF4,
0xFFF83CFB,0x49FFFFFF,0xBFEFFB8B,0x3BF8FFF4,
0xF0C00EDF,0x4AFFFFFF,0xBFEFFB86,0xBFE80A8B,
0xBF197A89,0xBFEFFB81,0xBFFFFB8B,0x6FFFFFFF,
0xF3000FDF,0xF7C00CFF,0xBFEFFB89,0x3BF83FF4,
0xFFF9CCFB,0x6FFFFFFF,0xF300109F,0xF7C00CFF,
0xFFC0021F,0x6FFFFFFF,0xFFC0021F,0x6FFFFFFF,
0x6FFFFFFF,0x00000000,0x00000000,0x00000000
#if 0
,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000,
0x00000000,0x00000000,0x00000000,0x00000000

#endif

}

0 项奖励
回复