ETPU engine control CRANK problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ETPU engine control CRANK problem

2,133件の閲覧回数
haizhougeng
NXP Employee
NXP Employee

Hi

 I am new to eTPU/eTPU2 usage.

I have followed both AN3769SW and AN47908SW to set up my project on MPC5777C EVB. Toothgen function works well. CRANK and CAM signal can be observed by oscilloscope.  But the CRANK function don't work well. I find the state of CRANK always stay in Initial State, FS_ETPU_CRANK_SEEK (AN47908SW )or FS_ETPU_CRANK_BLANK_TIME(AN3769SW).

I have tried many types of configuration but never let the state of CRANK change. I think it shouldn't be so hard, but I don't know waht can I do next.

Today I try the same code on MPC5746R board. It works well. Is there some difference between MPC5746R and MPC5777C when config ETPU?

 

Thanks in advance.

Best regards

etpu2   #engine control etpu mpc5777c‌

0 件の賞賛
返信
1 返信

1,907件の閲覧回数
haizhougeng
NXP Employee
NXP Employee

OK. I have fixed this issue. For MPC5777C, I have to config IGF if I use EPTUx as input. And if I follow AN3769, I muse config EPTU0 as crank channel.

0 件の賞賛
返信