Hi Dinakaran,
I can't see problem on my side.
I configured the eSCI in this way:
And then I simply wrote 0x0 to data register, so payload bits are written as 0 and TN (bit 8) is also 0.
I can measure pulse 0.52ms on oscilloscope. I'm configured baud rate 19200, so 1 start bit + 9 data bits gives:
10*52us = 520us.
Everything is correct from my point of view.
Regards,
Lukas