EMIOS Initialization issues in MPC5604s

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMIOS Initialization issues in MPC5604s

3,709 Views
mhogun
Contributor I

Hi All,

I am using MPC5604s controller. 

I am using EMIOS0 Channel 23 as Modulus Counter Buffered mode.To generate 125Hz frequency.

Below is my configurations:

/* Disable prescaler */
EMIOS_0.CH[CounterBus].CCR.B.UCPEN = 0;

/* Period = 8000(0-7999) clocks (8 msec) */
EMIOS_0.CH[23].CADR.R = 7999;

/* Modulus Counter Buffered (MCB) */
EMIOS_0.CH[23].CCR.B.MODE = 0x50;

/* Use internal counter as time base */
EMIOS_0.CH[23].CCR.B.BSL = 0x03;

/* Set channel prescaler to divide by 1 */
EMIOS_0.CH[23].CCR.B.UCPRE = 0x00;

/* Enable prescaler */
EMIOS_0.CH[23].CCR.B.UCPEN = 1;

/* Freeze channel counting when in debug mode */
EMIOS_0.CH[23].CCR.B.FREN =1;

I am using EMIOS0 Channel 21 in OPWMB mode.

Below line is used to disable the channel 21 in initialization function.

EMIOS_0.UCDIS.R |= (((uint32_t) 0x01 << 21));

The following line is used to set the PWM with 0% duty cycle.

EMIOS_0.CH[21].CADR.R = 7999;


EMIOS_0.CH[21].CBDR.R = 7999;

/*Enable  channel 21 */

EMIOS_0.UCDIS.R &= (~((uint32_t) 0x01 << 21));


/* Use Counter Bus A */
EMIOS_0.CH[21].CCR.B.BSL = 0x00;

/* Polarity-leading edge sets output/trailing clears */
EMIOS_0.CH[21].CCR.B.EDPOL = 0x01;

/* Mode is OPWM Buffered */
EMIOS_0.CH[21].CCR.B.MODE = 0x60;

/* Enable Output Update as it was disabled in pwm_init */
EMIOS_0.OUDR.R &= (~((uint32_t) 0x01 << 21));

The Channel 21 is connected to the LED.

The Issue is My LED is Blinks and OFF when i use the above configurations .

I want to Turn OFF my LED when i load below values to the both CADR and CBDR.

EMIOS_0.CH[21].CADR.R = 7999;
EMIOS_0.CH[21].CBDR.R = 7999;

Kindly help me to resolve the above issue.

Thanks in Advance.

Regards

Mohan raj.

0 Kudos
Reply
6 Replies

3,361 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Mohan,

Not sure of the issue.

Assuming the EDPOL=1 then setting

EMIOS_0.CH[21].CADR.R = 7999;

EMIOS_0.CH[21].CBDR.R = 7999;

will produce 0% duty. Output is set low.

 

If you set

EMIOS_0.CH[21].CADR.R = 0;

EMIOS_0.CH[21].CBDR.R = 7999;

100% duty is generated. Output is set high.

 

Check if the eMIOS channel is configured properly using a debugger. Also try to do not use UCDIS register within an initialization.

BR, Petr

0 Kudos
Reply

3,361 Views
mhogun
Contributor I

Hi Petr,

Thanks for the support.

I have checked eMIOS configuration by using debugger,it is configured properly.

Also not used UCDIS register within an initialization.

But the Issue is  LED is Blinks and OFF still.

Can you send me example code for initialization of eMIOS Channels.

Thanks in Advance.

 

Regards

Mohan raj.

0 Kudos
Reply

3,361 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Mohan,

The AN2865 (http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf) shows eMIOS OPWMB setting.

This demo code is also located in CodeWarrior 2.x installation, see it in [CW_installation]\(CodeWarrior_Examples)\560xS-CW\eMIOS-OPWM\. It works well.

BR, Petr

0 Kudos
Reply

3,361 Views
mhogun
Contributor I

Hi Petr,

I have checked the Sample code and also the referred the AN2865 document.

I am still getting the issue,

 

I will once again explain the issue,

I am using EMIOS0 Channel 23 as Modulus Counter Buffered mode.To generate 125Hz frequency.

The EMIOS0 Channel 21 use  EMIOS0 Channel 23 (Use Counter Bus A).

The EMIOS0 Channel 21  is used as OPWMB Mode connected to the LED.

When i load the any value(example:10,100,200)  for the first time to the  CADR register, the eMIOS gives the spike output.

The LED blinks for the first time and OFF.

When i load the any value or same as above  value (first time loaded value)  for the second time to the  CADR register, the eMIOS gives the constant output.

The LED is ON constantly.

The issue is eMIOS gives the spike output when we load the value for the first time.

This scenario happens for all the eMIOS0 and eMIOS1 channels

Kindly support me to solve the issue.

Thanks in Advance

With Regards

Mohanraj

0 Kudos
Reply

3,361 Views
mhogun
Contributor I

Hi Petr,

Please support to resolve the above mentioned issue.

Thanks in Advance

With Regards

Mohanraj

0 Kudos
Reply

3,361 Views
PetrS
NXP TechSupport
NXP TechSupport

try to use the FORCMB and enable global prescaler in last step during the initialization. This could help to not having first pulse.

See more in attached example.

BR, Petr

0 Kudos
Reply