EBI pull up/pull down configuration recommendation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EBI pull up/pull down configuration recommendation

1,309 Views
david_manna
Contributor I

Table 12-3 of Rev 4.0 of the MPC5553/MPC5554 Microcontroller Reference Manual lists the recommended pullup/pull down configuration for the external signals of the microcontroller when they are used as EBI signals. The column of the table titled "Pull" has a dash "--" entry for the address and data bus signals. What does the dash mean in regards to the recommended configuration for the pull up/pull down for the pin.

 

0 Kudos
Reply
1 Reply

1,254 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

a dash means no pullup/down is required for data and address lines, so it can be disabled in SIU.PCRs setting when configuring pad for EBI functionality.

BR, Petr

0 Kudos
Reply