EBI pull up/pull down configuration recommendation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EBI pull up/pull down configuration recommendation

1,299件の閲覧回数
david_manna
Contributor I

Table 12-3 of Rev 4.0 of the MPC5553/MPC5554 Microcontroller Reference Manual lists the recommended pullup/pull down configuration for the external signals of the microcontroller when they are used as EBI signals. The column of the table titled "Pull" has a dash "--" entry for the address and data bus signals. What does the dash mean in regards to the recommended configuration for the pull up/pull down for the pin.

 

0 件の賞賛
返信
1 返信

1,244件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

a dash means no pullup/down is required for data and address lines, so it can be disabled in SIU.PCRs setting when configuring pad for EBI functionality.

BR, Petr

0 件の賞賛
返信