EB tresos error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB tresos error

1,012 Views
Taresh
Contributor I

Hello,

I am getting error in existing sample configuration from MCU module related to MCU peripheral

during generation.

i had use sample plugins of MPC574XG_MCAL4_0_RTM_1_0_5_Sample_Application.

could anyone help me in this.

0 Kudos
Reply
1 Reply

984 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As the error states:

petervlna_0-1748502229956.pngpetervlna_0-1748502229956.png

So add McuPeripherals to match the number 66 in MCU module:

Below is the example for S32K3 but the principle is the same for any uC.

petervlna_1-1748502390057.pngpetervlna_1-1748502390057.png

petervlna_2-1748502402937.pngpetervlna_2-1748502402937.png

Best regards,

Peter

0 Kudos
Reply