Diffrence between SCI and eSCI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Diffrence between SCI and eSCI

2,028件の閲覧回数
rajiilangovan
Contributor II

Hi friend,

            Kindly give me the diffrence between SCI and eSCI in MPc5674F. and also give one sample code

ラベル(1)
0 件の賞賛
返信
1 返信

1,704件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Quoting Wikipedia:

'The term "Serial Communications Interface" (SCI) was first used at Motorola around 1975 to refer to their start-stop asynchronous serial interface device, which others were calling a UART. '

The terms SCI and UART are synonyms.

Our specific module implementation eSCI, used on certain MPC56xx devices, offers 2 functionalities: UART and LIN.

Note that LinFlex module that is being used on the rest of MPC56xx is the different module (coming from JDP program), however offers the same functionalities (UART and LIN).

Simple example code you may find here, chapter 15 and 16:

http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf

0 件の賞賛
返信