Devkit MPC5744P External HV Power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Devkit MPC5744P External HV Power supply

1,957 Views
ajaysrinivasann
Contributor I

Hello!

I am trying to supply my devkit for MPC5744P with external 12V power supply through header J3 pin 1 connected to +12V and ground to pin 13. I have set the jumper J39 and set J13 to external 12V supply. The supply is made through a 12V battery. The problem is that there seems to be a lot of noise in the supply voltage when I supply through the header(high frequency variations of almost +/-4V). Is there any other jumper that I should be setting? I have no issues when supplying with the PWR in connector in the Devkit. The problem is only when I choose to supply using header J3.µC.png

Regards,

Ajay

Labels (1)
Tags (1)
3 Replies

1,823 Views
ajaysrinivasann
Contributor I

Hi, yes it is the same battery.

0 Kudos
Reply

1,823 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

OK, if you connect it over barrel connector PWR, there is additional capacitor in the way that apparently eliminates noise coming from switching regulator. I could be the reason

pastedImage_2.png

1,823 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, are you comparing the same battery connected over PWR in and J3 header?