Debugging after reset automatically using lauterbach debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging after reset automatically using lauterbach debugger

1,052件の閲覧回数
Ahmed_BEN_LAKHEL1234
Contributor II

I made a project configuration using CMM script to test my software on MPC5777. In the software there is a component that make a reset so it make the debug failed. In this case, I need your support through an example of script CMM that include this commands SYStem.Option.ResetDetection ; SYStem.Option.RESetBehavior to reconnect the debugger automatically to the selected Core ( in my case Core 2 IOP )

 

 

0 件の賞賛
返信
1 返信

1,021件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have already posted my thoughts at:

https://community.nxp.com/t5/Zephyr-Project/Debugging-after-reset-automatically-using-lauterbach-deb...

I suggest to continue with just one thread.

Best regards,

Peter