Debugger for MPC5746R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger for MPC5746R

1,326 Views
nickvt
Contributor I

I am currently using the Multilink Universal debugger in combination with Codewarrior IDE and the MPC5634m microcontroller.

Does anybody know if the Multilink Universal also supports the MPC5746R microcontroller or if i have to switch to the Multilink Universal FX ? I am also planning on using the S32ds IDE.

Labels (1)
0 Kudos
Reply
1 Reply

1,236 Views
martin_kovar
NXP Employee
NXP Employee

Hello Nick,

you do not have to buy Multilink Universal FX. It is possible to use Multilink Universal for MPC5746R debugging.

Regards,

Martin

0 Kudos
Reply