DEVKIT-MPC5748G - I cannot debug when use multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-MPC5748G - I cannot debug when use multilink

5,480 Views
zyz
Contributor III

When trying to enter debug mode,warning is show below and RESET (Pin-9) is always driven low(either the red or the yellow LED light up),bug my board can working ok when use OpenSDA;

Any ideas what I could do or check?

 

 

Connection from "127.0.0.1" via 127.0.0.1. Connection from port "57519" to 7224
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @1000000 (4 bytes)
Copyright 2018 P&E Microcomputer Systems,Inc.
Command Line :D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=1500 -rese?
P&E Interface detected - Flash Version 10.46
Flash Data in range 0x00FA0000-0x00FA0003.
Flash Data in range 0x00FA0008-0x00FA0013.
Flash Data in range 0x01000000-0x01000167.
Flash Data in range 0x01001000-0x010010B3.
Flash Data in range 0x01002000-0x01002BCB.
Flash Data in range 0x01002BD0-0x0100897F.

CMD>RE

Initializing.

Device IDCODE is $00000000
Device ID revision is $00000000

Device IDCODE is $00000082
Device ID revision is $00000000

Device IDCODE is $00000000
Device ID revision is $00000000

Device IDCODE is $00000082
Device ID revision is $00000000

Device IDCODE is $00000000
Device ID revision is $00000000

Device IDCODE is $00000082
Device ID revision is $00000000
Cannot enter background mode. Check connections.
Error Resetting device for programming.

Device IDCODE is $00000000
Device ID revision is $00000000

Device IDCODE is $00000082
Device ID revision is $00000000

Starting reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\s32e200_mpc574xg.mac) ...
REM This script is compatible with MPC574xG devices.
REM Clean GPRs to remove residual data after using algorithm
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
Error : Error in ONCE status register during instruction execution.
REM Initialize all of the Main SRAM - 768KB
Initializing RAM from $40000000 to $400BFFFF.
Initializing Ram Block 0x40000000-0x400BFFFF.

Reset script (D:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\s32e200_mpc574xg.mac) completed.

MPC574xG Device detected.

PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session.

 

0 Kudos
Reply
12 Replies

5,472 Views
zyz
Contributor III

Yes, I have run this board and everything is fine when I use Open SDA

0 Kudos
Reply

4,474 Views
Lloyd
Contributor I

I get the same question when I use the OPENSDA,Error :Error in ONCE status register during instruction execution.Could you please tell me the answer for the question? Thank you!

0 Kudos
Reply

5,475 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, have you had this board ever running?

0 Kudos
Reply

5,471 Views
zyz
Contributor III

Yes, I have run this board and everything is fine when I use Open SDA

0 Kudos
Reply

5,461 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

So it works with OpenSDA but doesn't work over JTAG connector, correct?

davidtosenovjan_0-1622121424349.png

Have you connected 12V external supply over barrel connector?

0 Kudos
Reply

5,453 Views
zyz
Contributor III

Yes, when I use OpenSDA, it works normally, both for debugging and programming, but when I use JTAG, it cannot be programmed and debugged. I have tried both external 12V power supply and USB power supply

0 Kudos
Reply

5,426 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just checked it here and it works fine. Here is the configuration.

davidtosenovjan_0-1622274032229.png

 

 

 

0 Kudos
Reply

5,378 Views
zyz
Contributor III

I only have one MULTILINK at present, but the project is urgent. can I directly use the OpenSDA INTERFACE/JTAG CONNECTOR on the DEVKIT board as a debugger to debug my other boards?

0 Kudos
Reply

5,379 Views
zyz
Contributor III

I checked, my configuration is the same as yours, I think my mutilink may be broken.

0 Kudos
Reply

5,359 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You could try to ask PeMicro over their forum:

http://www.pemicro.com/forums/index.cfm

 

Maybe they could whether some issue exists with their device.

0 Kudos
Reply

5,428 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you specify DEVKIT revision? It should be stated on label from a bottom of the board.

0 Kudos
Reply

5,380 Views
zyz
Contributor III

My DEVKIT  revision is Rev D1

0 Kudos
Reply