DEVKIT-MPC5744P SB_RSTb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEVKIT-MPC5744P SB_RSTb

3,536 次查看
236
Contributor I

I have a problem to use external 12v.

When I input 12v, then the SB_RSTb indicator is turned on with little noise sound.

I think it's because of wrong connection between pins.

Now i disconnect them, but it was still indicating SB_RSTb.

I need some guide to solve the trouble.

 

标记 (1)
0 项奖励
回复
8 回复数

3,518 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

When I input 12v, then the SB_RSTb indicator is turned on with little noise sound.

It means your device is held in reset.

Are you able to connect via JTAG?

Did you followed quick start guide?

https://www.nxp.com/document/guide/getting-started-with-the-devkit-mpc5744p:NGS-DEVKIT-MPC5744P

Best regards,

Peter

0 项奖励
回复

3,494 次查看
236
Contributor I

Thanks, Peter.

Do i need to update firmware?

I've never used JTAG before.

So... may i get your guide about tools or something?

 

0 项奖励
回复

3,478 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am now confused.

So how do you update the code in micro?

Did you programmed anything into micro?

I am not sure if there is any guide regarding tools, there will be one for each from each vendor.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475

best regards,

Peter

0 项奖励
回复

3,449 次查看
236
Contributor I

I'm sorry. I misunderstood your previous reply.

I used micro USB to update the code.

I thought JTAG in your answer is about J11.

Anyways, i can connect via JTAG, then how can i solve this problem?

0 项奖励
回复

3,417 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Ok, once you connect with JTAG, is the reset released and you can debug the code?

Or is the connection not established because reset is still active?

Best regards,

Peter

0 项奖励
回复

3,408 次查看
236
Contributor I

The connection not established because reset is still active.

0 项奖励
回复

3,384 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, reset should be released once stable voltages are provided.

Can you check whether the voltages are in datasheet specified range? Just to be sure you didn't burn the board. There should be no issue if the jumpers are placed correctly.

petervlna_0-1712137543551.png

Best regards,

Peter

 

0 项奖励
回复

3,447 次查看
236
Contributor I

Together, I did powering selection settings(J44,J45,J43) to External 12V Power Supply.

0 项奖励
回复