DEVKIT-MPC5744P OpenSDA Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEVKIT-MPC5744P OpenSDA Flash

ソリューションへジャンプ
2,881件の閲覧回数
markusransberge
Contributor III

Hi,

I got a question about the new DEVKIT-MPC5744P's OpenSDA USB MCU, just to make sure:

Is it possible to flash .srec files onto the non volatile memory part of the main chip via the OpenSDA MCU or not? (There is no MSD programmer, right?) I only get to the bootloader drive to reflash the MCU itself (I guess), but using that for my compiled .srec files results in an endless "Programming..." state which you can read in the text file inside the bootloader drive. So that's probably not the right way to do it.

Thank you.

PS: Using JTAG I can program the main chip flawlessly, but I'd like to use the USB port if possible.

0 件の賞賛
返信
1 解決策
2,482件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi markusransberger‌,

Please check this out: https://community.nxp.com/thread/455356 

Hope it address your question.

Best regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,483件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi markusransberger‌,

Please check this out: https://community.nxp.com/thread/455356 

Hope it address your question.

Best regards,

Daniel

0 件の賞賛
返信
2,482件の閲覧回数
markusransberge
Contributor III

Thanks Daniel,

I actually got it running like 5 minutes ago. I was missing the RAppID bootloader on my board, so I just flashed the rbf file (MPC5744P_DEVKIT.rbf) and now it works just like your tutorial.

Thanks again.

0 件の賞賛
返信