DEVKIT-MPC5744P CAN PAL does not callback when add send call

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEVKIT-MPC5744P CAN PAL does not callback when add send call

1,631 次查看
jupiter
Contributor I

Hi friends,

my board is devkit-mpc5744p rev E1. There is a problem when adding sending call to CAN0, there is no received or sended complete callback triggered any more.

what is the context of my code and board is:

1.use CAN0 for receiving and sending with PB0 and PB1 on board, jumper J174 set to 4-6 and 3-5.

2.use USB power.

3.send 0x210 frame every 1 second.

Had anybody have the same problem? You can try my code on your board.

0 项奖励
回复
2 回复数

1,625 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I tried your example and it worked fine, but I used SBC's CAN transceiver and so external 12V to power a board, with board connected to PCAN tool. It should work with USB power too, but if you connect PB0/PB1 to headers, do you have these CAN TX/RX signals connected  to external transceiver and this transceiver via CAN bus to other CAN node, so a transmitted message can be ACKed? Not sure of further connection you have. Where PB0/PB1 are connected to? Check if your external CAN transceiver is functional.

BR, Petr

0 项奖励
回复

1,620 次查看
jupiter
Contributor I

Hi Petr,

I have found the problem, there is no external transceiver connected to PB0/PB1. It had been resolved by using SBC's CAN. The program is running happily now. Thanks for your help.     

BR, Semon

0 项奖励
回复