DEVKIT-MCP5744P connector spacing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEVKIT-MCP5744P connector spacing

1,873 次查看
nekvt
Contributor III

Hello,

I would like to ask you if there is some documentation about physical dimensions of expansion connectors of the DEVKIT-MPC5744P. I would like to design a expansion board for it to test out functionalities with our HW and I could not find any documents about physical dimensions. I need to incorporate all connector J1-6. As I understood J1-4 are Arduino Uno compatible, but the other ones are extra.

Thank you so much in advance.

Best regards,

Tomas

0 项奖励
回复
2 回复数

1,845 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, connectors used on the boards are following:

J1,J3,J4 = CON 2X8 SKT TH 100MIL CTR 340H SN 118L
Manufacturer Part Number is JT254-D180-850-210-001

J2,J5,J6 = CON 2X10 SKT TH 100MIL CTR 340H SN 118L
Manufacturer Part Number is JT254-D180-850-208-001

 

0 项奖励
回复

1,839 次查看
nekvt
Contributor III

Hi,
sorry for misunderstanding, I meant information about connector spacing, i.e. the position of pin 1 of connectors J1-6. I would like to design a shield for the DEVKIT and because of that I need the to know positions of the pins on this board.

Thanks so much for the answer.

Best Regards,

Tomas

0 项奖励
回复