MPC5748G windiss simulator - GDB-server???

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5748G windiss simulator - GDB-server???

1,031 次查看
rami_rosenbaum
Contributor II

Hi,

I'm working on the NXP MPC5748G board and want to develop on the windiss simulator as well.

Does it have a GDB-server? Very little info on the net...

This is how I'm running windiss:

PS C:\> windiss -tPPC C:\WindRiver\diab\5.9.4.8\example\powerpc\bubble.out
Initial array: 10 9 8 7 6 5 4 3 2 1
Number of tests: 90
Sorted array:  1 2 3 4 5 6 7 8 9 10
windiss: Task finished, exit code: 0, Instructions executed: 19378
windiss: Interrupts were never enabled

Thanks.

标记 (3)
0 项奖励
回复
0 回复数