Cyclone FX error $00000007

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cyclone FX error $00000007

1,338 Views
Harrisfan
Contributor I

Hello,

I am using the Cyclone FX to do an offline program flashing of the MPC5744 chip, after making sure the hardware is connected correctly.

Script setup:CM - SS - EM - PM - VC

However, when writing to the controller through the 14PIN port, there is a problem of not being able to enter or exit debug mode

Please help me to solve it, thanks!

0 Kudos
Reply
1 Reply

1,289 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Not sure what do you mean by offline programming.

Are you using NXP evaluation board, or you own board design?

There should be no issue connecting to this micro when you have not secured it via censorship and your voltages are in datasheet specified range.

Best regards,

Peter

0 Kudos
Reply