Continuous ADC conversion for 5746R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Continuous ADC conversion for 5746R

1,316 Views
supra0309
Contributor I

Hi,

Here's my code modified from example adc_pal_mpc5746r.

#define ADC_CHAN_INDEX_CONNECTED2 (2)
#define ADC_CHAN_INDEX_CONNECTED1 (1)
#define ADC_CHAN_INDEX_CONNECTED0 (0)
/* Flag used to store if an ADC PAL conversion group has finished executing */
volatile bool groupConvDone = false;
/* Flag used to store the offset of the most recent result in the result buffer */
volatile uint32_t resultLastOffset = 0;
void adc_pal1_callback00(const adc_callback_info_t * const callbackInfo, void * userData)
{
    (void) userData;
    groupConvDone = true;
    resultLastOffset = callbackInfo->resultBufferTail;
}

/*
* Description: Convert a float to null terminated char array
*/
static void floatToStr (const float *srcValue, char *destStr, uint8_t maxLen);
/*!
\brief The main function for the project.
\details The startup initialization sequence is the following:
* - startup asm routine
* - main()
*/
int main(void)
{
    status_t status;
    uint8_t selectedGroupIndex;
    const uint16_t adcMax = (1u << 12u); /* Resolution is 12bits for all ADC instances */
    float resVolts0;
    float resVolts1;
    float resVolts2;
    /* Buffer used to store processed data for serial communication */
    char msg[255] =
    { 0, };

    status = CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
    g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
    DEV_ASSERT(status == STATUS_SUCCESS);

    status = CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);

    DEV_ASSERT(status == STATUS_SUCCESS);
    /* Initialize pins
    * - See PinSettings component for more info
    */
    PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
    /* Initialize the ADC PAL
    * - See ADC PAL component for the configuration details
    */
    status = ADC_Init(&adc_pal1_instance, &adc_pal1_InitConfig0);
    DEV_ASSERT(status == STATUS_SUCCESS);
    /***************************************************************
    * Part 1 of the example: software triggered conversion group
    ***************************************************************/
    selectedGroupIndex = 0u; /* Select the index of a SW triggered group of conversions (see ADC PAL component) */
    /* Start the selected SW triggered group of conversions */
    status = ADC_StartGroupConversion(&adc_pal1_instance, selectedGroupIndex);
    DEV_ASSERT(status == STATUS_SUCCESS);
    /* Called only for demonstration purpose - it is not necessary and doesn't influence application functionality. */
    status = ADC_StartGroupConversion(&adc_pal1_instance, 1u); /* Starting another SW triggered group while other is      running will return BUSY. */
    /* Do not place any breakpoints or run step-by-step between the start of the first conversion group
    * at line ADC_StartGroupConversion(&adc_pal1_instance, selectedGroupIndex) and line with DEV_ASSERT(status

    == STATUS_BUSY).
    * Otherwise the DEV_ASSERT will fail because of timing restrictions: previous conversion list finishes execution              before the second call to
    * ADC_StartGroupConversion() => will return different status than expected. */
    DEV_ASSERT(status == STATUS_BUSY);
    uint8_t iter = 0;
    while(true)
    {
        /* Wait for group to finish */
        if(groupConvDone == true)
        {
        resVolts0 = ((float) adc_pal1_Results00[ADC_CHAN_INDEX_CONNECTED2] / adcMax) * VREF;
        floatToStr(&resVolts0, msg, 5);
        resVolts1 = ((float) adc_pal1_Results00[ADC_CHAN_INDEX_CONNECTED1] / adcMax) * VREF;
        floatToStr(&resVolts1, msg, 5);
        resVolts2 = ((float) adc_pal1_Results00[ADC_CHAN_INDEX_CONNECTED0] / adcMax) * VREF;
        floatToStr(&resVolts2, msg, 5);                                 *****I set breakpoint at here to watch 3 resVolt value, if there's                                                                                                  no breakpoint, it will be empty in variables.

        /* Reset flag for group conversion status */

        groupConvDone = false;
        iter ++;
        OSIF_TimeDelay(100);
        /* Restart the SW triggered group of conversions */
        status = ADC_StartGroupConversion(&adc_pal1_instance, selectedGroupIndex); /* Restart can be avoided if SW            triggered group is configured to run in continuous mode */
        DEV_ASSERT(status == STATUS_SUCCESS);
        }
    }
    status = ADC_Deinit(&adc_pal1_instance);
    DEV_ASSERT(status == STATUS_SUCCESS);

    for(;;)

    {
        if(exit_code != 0)

        {
            break;
        }

    }

    return exit_code;

}

I've already finished pinsettings and component inspector in adc_pal1 (both are shown in figure), now I can receive voltage conversion results once from motherboard shown in variables.But I need to receive changing voltage conversion results continuously, how can I make it work? Thanks.

Best Regards,

Xantia

pastedImage_31.pngpastedImage_32.pngpastedImage_33.pngpastedImage_35.pngpastedImage_36.png

Labels (1)
0 Kudos
Reply
0 Replies