Compiling MCAL example for MPC5748G with gnu powerpc-eabi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiling MCAL example for MPC5748G with gnu powerpc-eabi

2,567 Views
andibavaria
Contributor II

Hi,

I'm trying to run the MCAL example on a MPC5748G Dev Kit Board. It seems that the MCAL example is only configurable for the Green Hills or WindRiver Compiler. 

Is it possible to run the MCAL example with the standard GNU Compiler (powerpc-eabi) from the S32 Design Studio installation?

Has anyone already run MCAL or AutosarOS with the powerpc-eabi compiler on the MPC5748G? (launch.bat etc. configured)

Thanks for the help!

2 Replies

2,373 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

MCAL is officially tested for GreenHills and Windriver compilers.

Peter

2,373 Views
andibavaria
Contributor II

ok, so no chance to run it with other compilers.... would be too much hustle than simply get a GrennHills/Windriver compiler and everything (makefile, scripts, examples) is already working.

0 Kudos
Reply