Codewarrior code smaples for MPC5668G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior code smaples for MPC5668G

2,676 Views
ravikiranbhairu
Contributor II

Hello All,

 

Where can I find the Codewarrior expert codes for MPC5668G EVB to begin with?

 

Regards,

Ravikiran

Labels (1)
Tags (1)
5 Replies

2,426 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am attaching such a base project for MPC5668G device.

Also pay attention to following appnote that however uses GHS environment for these examples:

http://cache.freescale.com/files/32bit/doc/app_note/AN4241.pdf

http://cache.freescale.com/files/32bit/doc/app_note/AN4241SW.zip

2,426 Views
ravikiranbhairu
Contributor II

Hello David,

Thank you very much for the Response.

Do you have hands-on experience with MPC5668G EVB and Codewarrior? I received the EVB 2 days before. I havent changed any Jumper settings. Tried to run a simple blink led code to blink the user LED's. It did not work. Do i need to make any change in Jumper Settings?

0 Kudos
Reply

2,426 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it works normally. But it is needed to connect pin PH10 to user led header (P15) by wire.

0 Kudos
Reply

2,426 Views
zhoutianyuan
Contributor I

Hi,Ravikiran.

   

     Maybe you can find some examples when settingup the software CodeWarrior. The possible path is "C:\Program Files (x86)\Freescale\CW for MPC55xx and MPC56xx 2.10\(CodeWarrior_Examples)". Good luck

2,426 Views
ravikiranbhairu
Contributor II

Hello Zhou,

Thank you. There are many example projects available in the path you have mentioned. But not specifically for MPC5668G EVB. May be these examples could help me in understanding basics. Thank you again,

0 Kudos
Reply