Codewarrior code smaples for MPC5668G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior code smaples for MPC5668G

2,835件の閲覧回数
ravikiranbhairu
Contributor II

Hello All,

 

Where can I find the Codewarrior expert codes for MPC5668G EVB to begin with?

 

Regards,

Ravikiran

ラベル(1)
タグ(1)
5 返答(返信)

2,585件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am attaching such a base project for MPC5668G device.

Also pay attention to following appnote that however uses GHS environment for these examples:

http://cache.freescale.com/files/32bit/doc/app_note/AN4241.pdf

http://cache.freescale.com/files/32bit/doc/app_note/AN4241SW.zip

2,585件の閲覧回数
ravikiranbhairu
Contributor II

Hello David,

Thank you very much for the Response.

Do you have hands-on experience with MPC5668G EVB and Codewarrior? I received the EVB 2 days before. I havent changed any Jumper settings. Tried to run a simple blink led code to blink the user LED's. It did not work. Do i need to make any change in Jumper Settings?

0 件の賞賛
返信

2,585件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it works normally. But it is needed to connect pin PH10 to user led header (P15) by wire.

0 件の賞賛
返信

2,585件の閲覧回数
zhoutianyuan
Contributor I

Hi,Ravikiran.

   

     Maybe you can find some examples when settingup the software CodeWarrior. The possible path is "C:\Program Files (x86)\Freescale\CW for MPC55xx and MPC56xx 2.10\(CodeWarrior_Examples)". Good luck

2,585件の閲覧回数
ravikiranbhairu
Contributor II

Hello Zhou,

Thank you. There are many example projects available in the path you have mentioned. But not specifically for MPC5668G EVB. May be these examples could help me in understanding basics. Thank you again,

0 件の賞賛
返信