Checker Core running status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Checker Core running status

1,680件の閲覧回数
AnnaKoteswarara
Contributor I

Hi ,

I am using the Freescale micro  Cobra 55 controller, MPC5777C ,  for my application.

 

1. Is there any way i can read the Checker Core running status from any registers instead of SIU_LOCKSTEP register where it shows only Lock step core is enabled or not? But if i wanted to know even though it is enabled , how to make sure that it is running or not?

 

 

2. If there is any failure in the Checker core, i need to check only FCCU status?

ラベル(1)
0 件の賞賛
返信
1 返信

1,359件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) There is FCCU non-critical fault 42 indicating checker core is disabled.

2) Yes, faults 10 and 11.

0 件の賞賛
返信