Checker Core running status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Checker Core running status

1,682 Views
AnnaKoteswarara
Contributor I

Hi ,

I am using the Freescale micro  Cobra 55 controller, MPC5777C ,  for my application.

 

1. Is there any way i can read the Checker Core running status from any registers instead of SIU_LOCKSTEP register where it shows only Lock step core is enabled or not? But if i wanted to know even though it is enabled , how to make sure that it is running or not?

 

 

2. If there is any failure in the Checker core, i need to check only FCCU status?

Labels (1)
0 Kudos
Reply
1 Reply

1,361 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) There is FCCU non-critical fault 42 indicating checker core is disabled.

2) Yes, faults 10 and 11.

0 Kudos
Reply