Changing System Clock Frequency can not speed up processing speed when using MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing System Clock Frequency can not speed up processing speed when using MPC5744P

1,320件の閲覧回数
bruceye
Contributor II

Hi :

I have a problem to speed up the calculation of the MPC5744P by changing the system clock frequency.

First of all, 16 MHz IRCOSC was used as the system clock ( MC_ME.RUN0_MC.B.SYSCLK = 0;)and I tested  the time for MPC5744P to process a formula, it takes around 100us (Testing by PIT) .Then I used the primary PLL (PHI) as the source of system clock ( MC_ME.RUN0_MC.B.SYSCLK = 2), so the system clock frequency is supposed to be 160MHZ. But the processing time stayed unchanged .

Could you give me some advice on why I cannot speed up processing speed by changing  system clock frequency ?

Thanks

Bruce

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,077件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is not supposed to be changed. PIT uses IRC as clock source:

pastedImage_4.png

pastedImage_5.png

0 件の賞賛
返信

1,076件の閲覧回数
bruceye
Contributor II

Hi David:

Thank you for your reply.Probably because I did not express my problem clearly that you misunderstood what I mean .

My problem is I can not speed up the microcontroller's speed by changing the clock source of the system clock(from 16Mhz to 160Mhz).Using PIT was just to detect how long it takes for a microcontroller to run a program.The result is that  I can not speed up processing speed by changing  system clock frequency.

So could you please give me some advice again ?

Thank you

Bruce

0 件の賞賛
返信

1,077件の閲覧回数
xiaopi
Contributor II

hi,i have the same problem just like you faced.coule you give you email or wechat,i really want to know how to speed up the microcontroller's speed.

my email is 382215239@qq.com,you can contact me also.

0 件の賞賛
返信

1,077件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I see.

Please pay attention to following example code, functions SysClk_Init and PeriClkGen_init:

Example MPC5744P PinToggleStationery S32DS 

Hope it helps.