Cannot start a network interface on MPC5748G (lwIP stack)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot start a network interface on MPC5748G (lwIP stack)

4,422件の閲覧回数
pmrlcbtcphtzjdq
Contributor III

Hallo!

I am struggling with lwip and a UDP connection. I am running it on a board with freeRTOS.

First, I added freeRTOS form the component list. 

Next, I added the tcpip component from the componnent library - it adds the lwIP. The settings of this component are in the included picture.

Third step was set up the PINs in the pin_mux GUI configuration (I am using NXP lwip ping example as a reference - it has been working properly). I am attaching the pin out in the image below.

Fourth step was to create a task for the OS and write few simple NETCONN API commands to send UDP packages. They seem to work (return value is equal to err_ok) up to the netconn_send() command.

The UDP packages are never sent though. I figured out, that it is because the initialisation doesn't work and netconn_send() has no network interface to work with. I cannot get a working network interface.The tcipip_init() function is supposed to create a netif and it fails - by the debbuging I figured out that the netif is always NULL. I tried to add a network interface myself, but it also fails.

It looks that I should enable somewhere some hardware options somewhere, or change the initialisation procedure - the code seems correct, and is similar to NXP example.... Does anybody know how to solve the problem of missing netif?

All my code is inside an InitTask - a Task with hight priority that will run on the power up. I am attaching two code examples that fail. I would be really grateful for any comments or ideas!

My first approach (fails on tcpip_init(), precisely speaking on netif_add() that is called from tcpip_init )

struct netconn *conn;
struct netbuf *buf;
ip_addr_t dst_addr;
ip_addr_t board_addr;
char *send_data;
char text[] = "MPC5748G";
int i;
tcpip_init(NULL, NULL);
err_t connection_err, send_err, bind_err;
PINS_DRV_SetPins(PTB, 0x1000); //PB12
vTaskDelay( 1000 / portTICK_PERIOD_MS );
PINS_DRV_ClearPins(PTB, 0x1000); //PB12
u16_t dst_port = 7000;

/* create a new connection */
conn = netconn_new(NETCONN_UDP);

/* set up the IP address of the remote host */

dst_addr.addr = inet_addr("192.168.0.7");
board_addr.addr = inet_addr("192.168.0.200");
/* connect the connection to the remote host */
bind_err = netconn_bind(conn, &board_addr, 44444 );
if (bind_err== ERR_OK) { PINS_DRV_SetPins(PTA, 0x1000); } //PA12
connection_err = netconn_connect(conn, &dst_addr, dst_port);

if (connection_err== ERR_OK) { PINS_DRV_SetPins(PTA, 0x2); } //PA1

/* create a new netbuf */
buf = netbuf_new();
netbuf_ref(buf, text, 9);

for(i=0;i<5;i++){
/* send the arbitrary data */
send_err = netconn_send(conn, buf);

if (send_err == 0) { PINS_DRV_TogglePins(PTE, 0x40) ;} //PE6
vTaskDelay( 500 / portTICK_PERIOD_MS );
}

I also tried to add the network interface manually with this code, but this also fails:

struct netconn *conn;
struct netbuf *buf;
ip_addr_t dst_addr, addr, gw, netmask;
struct netif* my_netif;
char *send_data;
char text[] = "MPC5748G";
int i;
/* IP default settings*/
IP4_ADDR(&addr, 192, 168, 0, 200);
IP4_ADDR(&gw, 192, 168, 0, 1);
IP4_ADDR(&netmask, 255, 255, 255, 0);
err_t my_ip_init(struct ip_addr *addr,
struct ip_addr *netmask,
struct ip_addr *gw,
err_t (* init)(struct netif *netif),
err_t (* input)(struct pbuf *p, struct netif *netif));
tcpip_init(NULL, NULL);
netifapi_netif_add(&my_netif, &addr, &netmask, &gw, NULL, enet_ethernetif_init, tcpip_input);

/* register the default network interface */

netif_set_up(&my_netif);
netif_set_default(&my_netif);

I am attaching my set up of the pins form pin_mux, and the configuration of the tcpip component:

 

0 件の賞賛
返信
2 返答(返信)

4,351件の閲覧回数
lixu
Contributor II

Hi, 

I also want to change the IP address. It can ping but cannot transmit data.

Have you solved your problem?

Thanks and best regard,

lixu

0 件の賞賛
返信

4,402件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This is question on IwIP stack and it is not MCU related.

Maybe someone from community can help you.

 

best regards,

Peter

 

0 件の賞賛
返信