Can't I write the UTEST area using Flash driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't I write the UTEST area using Flash driver?

1,485件の閲覧回数
jaejynshin
Contributor III

Dear Experts.

 

I am using MPC5777C.

I want to write JTag Password in the UTEST area through flash api which was based on flash driver.

But Verification Fail occurred during writing. 

Can't I write the UTEST area using Flash driver?

 

Thank you

Jaejyn

ラベル(1)
0 件の賞賛
返信
1 返信

1,311件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

The DCF records are not intended to be written via application SW.

User have to write them during development phase. (not in field)

For this purpose use can use debugger (scripts) or via programmer machine in production.

Peter

0 件の賞賛
返信