Can't I write the UTEST area using Flash driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't I write the UTEST area using Flash driver?

1,493 Views
jaejynshin
Contributor III

Dear Experts.

 

I am using MPC5777C.

I want to write JTag Password in the UTEST area through flash api which was based on flash driver.

But Verification Fail occurred during writing. 

Can't I write the UTEST area using Flash driver?

 

Thank you

Jaejyn

Labels (1)
0 Kudos
Reply
1 Reply

1,319 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

The DCF records are not intended to be written via application SW.

User have to write them during development phase. (not in field)

For this purpose use can use debugger (scripts) or via programmer machine in production.

Peter

0 Kudos
Reply