Can not clear ECSM.ESR.R1BC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not clear ECSM.ESR.R1BC

1,870 Views
buzduganandrei
Contributor I

Hello NXP Community,

 

 I am developing some code to help verify the ECC's HW for RAM. For this I need to use the error injection mechanism and inspect the ESR.R1BC. While I do see that ECC has captured correctly the address and data of the error, (though the symptom bits are way off) and the R1BC is asserted, I can not clear the R1BC.

 I have the following algorithm :

 

//Load ECSM.EEGR.ERRBIT

//Set ECSM.EEGR.FR11BI

 

//Generate SEC
array[0] = 0xFFFFFFFF - u8Idx;
readBackData= array[0];

 

//Clear ECSM.EEGR.FR11BI

 

if (ECSM.ESR.R1BC == 0x1)
{
ECSM.ESR.R1BC = 0x1;

}
else
{
/*Nothing to do.*/
}

 

 To be more specifically, I can see the R1BC clear to 0, but after half a second it is put back to 1.I can clear it, if I deactivate the ECC 1-bit RAM reporting. But, later if I re-activate it, the R1BC automically sets (restores more like it) itself. I've looked through the errata, but I didn't find anything similar. This is for SPC5605B. Did anybody else run into this scenario ? if so, is there a way-around ?

Labels (1)
Tags (3)
1 Reply

1,746 Views
buzduganandrei
Contributor I

ECC mechanism corrects 1-bit errors internally, NOT in RAM. The correct data is passed to the core, but the RAM remains corrupted. Because of this, the original address with the error needs to be written with a good data.