Can LINFLEXD module sleep automatically when it receives LIN frame (ID = 0x3C, Data= 0x00)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LINFLEXD module sleep automatically when it receives LIN frame (ID = 0x3C, Data= 0x00)?

1,047 Views
ykp3036
Contributor I

Can LINFLEXD module sleep automatically when it receives LIN frame (ID = 0x3C, Data= 0x00, 0x11,0x11,0x11,0x11,0x11,0x11,0x11)?

that is the SLEEP instruction.

0 Kudos
Reply
1 Reply

1,036 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The go-to-sleep command is a diagnostic Master request frame (ID 0x3c) with the first data byte being 0x00. The go-to-sleep command is a broadcast message to all nodes on the bus. It signifies that the Lin bus is shutting down.
What the node does then is the application specific. There is no predefined behavior on the LINFlexD module. So no, LINFlexD does not automatically go to sleep.

BR, Petr

0 Kudos
Reply