Can LINFLEXD module sleep automatically when it receives LIN frame (ID = 0x3C, Data= 0x00)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can LINFLEXD module sleep automatically when it receives LIN frame (ID = 0x3C, Data= 0x00)?

298 次查看
ykp3036
Contributor I

Can LINFLEXD module sleep automatically when it receives LIN frame (ID = 0x3C, Data= 0x00, 0x11,0x11,0x11,0x11,0x11,0x11,0x11)?

that is the SLEEP instruction.

0 项奖励
1 回复

287 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The go-to-sleep command is a diagnostic Master request frame (ID 0x3c) with the first data byte being 0x00. The go-to-sleep command is a broadcast message to all nodes on the bus. It signifies that the Lin bus is shutting down.
What the node does then is the application specific. There is no predefined behavior on the LINFlexD module. So no, LINFlexD does not automatically go to sleep.

BR, Petr

0 项奖励