Can I add CAN-FD and Basic CAN on same network ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I add CAN-FD and Basic CAN on same network ?

4,620 次查看
Amit_Kumar1
Senior Contributor II

Hi

 

I had a doubt if I can add Basic CAN nodes and CAN-FD nodes on same network. Can I send messages from CAN-FD to Basic CAN? As per my understanding we can but wanted to make sure.

Thanks in advance.

 

Regards

Amit

标签 (1)
标记 (4)
2 回复数

4,248 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at chapter Compatibility of CAN and CAN FD in:

http://v2.can-newsletter.org/uploads/media/raw/a87bb7bf1088d89d558f5b22ced9099a.pdf

Regards,

Lukas

4,248 次查看
Amit_Kumar1
Senior Contributor II

Hi

After reading more about CAN and CAN-FD, I came to the conclusion that Basic CAN and CAN-FD can be present on same network and can communicate to one another provided CAN-FD is sending the Basic CAN frame. If Basic CAN Node detects CAN-FD frame , It will start transmitting error frames so no Node will be able to receive the CAN_FD frame.

Regards

Amit