Calypso 3M EEPROM emulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Calypso 3M EEPROM emulation

1,771 Views
neojung
NXP Employee
NXP Employee

Hello team,

 

Do we have EEPROM emulation driver demo project for Calypso 3M?

Currently driver demo does not have Calypso family's project.

 

Best regards,

Neo

Labels (1)
0 Kudos
Reply
1 Reply

1,564 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Neo,

I'm afraid that currently there's no such example. It will be necessary to write own definition of EE blocks in ee_block.h because it is different against other devices. There are examples for MPC5744P, MPC5746R, MPC5775K - all of them have data flash at address 0x80_0000. Then there's MPC5777C which has four 64KB block at address 0x0 (example is included in the package too) and MPC5748G/MPC5746C where you can use up to eight 16KB blocks at 0x00F9_0000.

Regards,

Lukas