MPC5606S PWM output without using a Unified Channel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5606S PWM output without using a Unified Channel

2,420 次查看
akhilprasad
Contributor III

In MPC5606S, can we get PWM output in any particular channel without using a Unified Channel(23,16,8).

标签 (1)
6 回复数

2,220 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

No, this is not possible for eMIOS channels 9-15. See Tables 9-2 and 9-3 of the Reference manual.

BR, Petr

2,220 次查看
akhilprasad
Contributor III

Thank you Petr. 

Is there any way i can get pwm output in eMIOSB channels 16 to 23 without using Unified channels(16 or 23).

I got pwm output when i configured unified channel 23/16. But i need to get output in channels(16 to 23) without using unified channels. Is it possible to do so ?

0 项奖励
回复

2,220 次查看
PetrS
NXP TechSupport
NXP TechSupport

Configure channels to OPWFMB mode which is available for all channels on eMIOS 1 module as per Table 9-3.

The internal channel counter is automatically selected as the time base when this mode is selected.

BR, Petr

0 项奖励
回复

2,220 次查看
akhilprasad
Contributor III

ok.. 

I configured channels in OPWMB mode.

Can u ples share me a code configuring channel in OPWMB and without using any unified channels.

0 项奖励
回复

2,220 次查看
PetrS
NXP TechSupport
NXP TechSupport

The OPWMB mode have to use other counter bus (channels 16 or 23). The OPWFMB mode does not...

Here is basic code for OPWFMB mode...

void initEMIOS(void) {

 

  EMIOS_1.MCR.B.GPRE= 63;     /* Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk*/

  EMIOS_1.MCR.B.ETB = 0;      /* External time base is disabled; */

  EMIOS_1.MCR.B.GPREN = 1;     /* Enable eMIOS clock */

  EMIOS_1.MCR.B.GTBE = 1;                         /* Enable global time base */

  EMIOS_1.MCR.B.FRZ = 1;                            /* Enable stopping channels when in debug mode */

}

 

void initEMIOSch(void) {       /* EMIOS CH : Output Pulse Width & Freq Modulation*/

                                /*           Provide 10KHz output (100usec period) */

                                /* Input clock is eMIOS clk of 1MHz (1 usec period)*/

  EMIOS_1.CH[17].CBDR.R = 99;      /* Period = 1 usec x (99+1) = 100 usec, 10KHz*/

  EMIOS_1.CH[17].CADR.R = 30;       /* Duty cycle  */

  EMIOS_1.CH[17].CCR.B.UCPRE = 0;  /* Channel counter uses divide by (0+1) prescaler */

  EMIOS_1.CH[17].CCR.B.UCPEN = 1; /* Channel counter's prescaler is loaded & enabled*/

  EMIOS_1.CH[17].CCR.B.EDPOL = 1;         /* Polarity is active high */

  EMIOS_1.CH[17].CCR.B.MODE= 0x58; /* Mode= 0PWFMB */

}

BR, Petr

0 项奖励
回复

2,220 次查看
akhilprasad
Contributor III

Thanks a lot Petr. The information was very much useful. I will try the code.

0 项奖励
回复