Cache HIT and Miss Latency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cache HIT and Miss Latency

1,955 Views
chaitanyakumarb
Contributor II

I am using MPC5777C, wanted to understand the cache HIT time and miss latency.

1) how do we compute these timings, are they standard times for all misses and hits?

2) what are the scenarios of cache flush?

are they  through

a) mtspr l1finv0 (for Data cache), mtspr l1finv1 (for instrcution cache) instruction

b) during cache replacement that is when Dirty bit is set and there is a cache miss detected or any other ways?

3) Invalidation of cache will results in cache flush also?

0 Kudos
Reply
1 Reply

1,896 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) If there is cache hit, there is access without wait states. If cache miss, access latency is given by access path to the target memory.

 

2) Both variants. Also there is instruction dcbf for that purpose.

 

3) No, invalidation is equal to flush only in write through mode. In the copy back mode, invalidation does not perform flush operation (i.e. does not copy line back if modified).

0 Kudos
Reply