CW11.1 for MPC56X Problem1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW11.1 for MPC56X Problem1

5,448件の閲覧回数
NXP_Hongyu
Contributor I

Capture.PNGwhen i installed the CW11.1, i can't create a new project for MPC56X, because i can't find relevant device

 

0 件の賞賛
返信
11 返答(返信)

5,441件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it was necessary to select "Qorivva" (this was a nickname for MPC5xxx devices in the past) during the  installation:

lukaszadrapa_0-1632307753339.png

To add support to existing installation, open Help -> Install New Software

and select:

lukaszadrapa_1-1632307858493.png

Regards,

Lukas

5,143件の閲覧回数
JOE_1209
Contributor III

Hi Lukas,

I am also using the chip MPC5602P and I have followed the instruction to update the Qorivva Support & MCU v11.1 Update for Qorivva. However, when I created a new project for MPC5602P,  the component inspector is blank. I assume there is no SDK S32PA support for MPC5602P? I also tried S32 design studio power architecture, the component inspector is blank as well

S32 Design Studio問題.PNG

Regards,

Joe

0 件の賞賛
返信

5,128件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, that's correct. There's no SDK for MPC56xx family of devices. We provided Autosar MCAL only:

https://www.nxp.com/design/automotive-software-and-tools/autosar:AUTOSAR-HOME

Regards,

Lukas

 

0 件の賞賛
返信

5,114件の閲覧回数
JOE_1209
Contributor III

Hi Lukas,

 

Thank you for the reply. I installed the files

1. STUDIO_14.0.0_2013-02-26

2. MPC560XP_MCAL4.0_RTM_1.0.0_signed

3. MPC560XP_MCAL4.0_RTM_HF1_1.0.0_signed

For the MCAL4.0 RTM, I installed them under the path of "C:\EB\tresos\plugins"

file directory.PNG

When I clicked file -> import -> Existing Project into Workspace on Tresos studio, I selected "MPC560XP_MCAL4.0_RTM_1.0.0_Integration_Application" as root directory. (which then be copied into workspace). Then I clicked SampleApplication (PA, XPC560XP), it prompted a warning showing T2D11M10I0R0 is not installed. Where should I move all the files with T2D11M10I0R0 ending? So the Tresos Studio can load the configuration.

EBtresos.PNG

My intent here is to only configure the low level driver and pin configuration. no need for OS.

 

Best Regards,

Joe 

0 件の賞賛
返信

5,010件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Joe,

I'm sorry for delayed response caused by Christmas holidays. This is for another team, so if it is still not resolved, please create new ticket here and it will be assigned to them:

https://support.nxp.com/

Thanks,

Lukas

0 件の賞賛
返信

5,006件の閲覧回数
JOE_1209
Contributor III

Hi Lukas,

Happy 2022, I created a new post and Nam is helping me with the issue

Thanks,

Joe

0 件の賞賛
返信

5,427件の閲覧回数
NXP_Leo
Contributor II

Hi 

I operate according to your instructions, i meet a new issue below:

Capture.PNG

I disable the 1.0.3 version of buildtools, then it can continue again, but i don't know whether this will influence my developpment.

0 件の賞賛
返信

5,425件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

That should be ok, it's just older version which is not needed.

Regards,

Lukas

0 件の賞賛
返信

5,409件の閲覧回数
NXP_Leo
Contributor II

Capture.PNG

MCU above is what i use, but i don't know which family i should select from item below:

Capture1.PNG

0 件の賞賛
返信

5,404件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you really have SPC5604P34/SPC560P40, you are talking to wrong company. These are parts from ST. Please contact www.st.com

Regards,

Lukas

0 件の賞賛
返信

5,420件の閲覧回数
NXP_Leo
Contributor II

Thanks for your support!

0 件の賞賛
返信