CMU with FCCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CMU with FCCU

跳至解决方案
1,891 次查看
mehmetkaradag
Contributor III

Hi, NXP engineers.

I am using MPC5777C.

i wanna get interrupt using FCCU if CMU_0_pll is damaged. Is there any aplication note or example about it. So which interrupt will code jump? FCCU or CMU?

mehmetkaradag_0-1684418058991.png

thanks for helps.

0 项奖励
回复
1 解答
1,870 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is there any application note or example about it.

No, as far as I know. It is simple settings of FCCU. For that I have AN here: Its the same module as for SPC5744P.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

So which interrupt will code jump? FCCU or CMU?

Well, there is no interrupt for CMU in INTC module. So  only FCCU can trigger such interrupt based on signals from CMU.

petervlna_0-1684478705570.png

 

Best regards,

Peter

在原帖中查看解决方案

1 回复
1,871 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Is there any application note or example about it.

No, as far as I know. It is simple settings of FCCU. For that I have AN here: Its the same module as for SPC5744P.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

So which interrupt will code jump? FCCU or CMU?

Well, there is no interrupt for CMU in INTC module. So  only FCCU can trigger such interrupt based on signals from CMU.

petervlna_0-1684478705570.png

 

Best regards,

Peter