CMU ISR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,943 Views
Amr_Awny
Contributor II

In CMU0, CMU3, CMU4 

the ISR of each fire 0x02, FLLI 

What are the values should be written in their division register in order to clear the ISR FLLI bit ?

 

CMU0

=160Mhz*16*4/16Mhz =640

LFREF = 640*0.95 = 608 --> 0x260

HFREF = 800*1.05 = 672 --> 0x2A0

MC_CGM_AC0_DC0=0x80010000

 

CMU3

=80Mhz*16*4/16Mhz =320

LFREF = 320*0.95 = 304 --> 0x130

HFREF = 320*1.05 = 336 --> 0x150

MC_CGM_AC0_DC2 = 0x80000000

 

CMU4

=80Mhz*16*4/16Mhz =320

LFREF = 320*0.95 = 304 --> 0x130

HFREF = 320*1.05 = 336 --> 0x150

MC_CGM_AC1_DC1= 0x80000000

Amr_Awny_0-1652285062870.png

 

0 Kudos
Reply
1 Solution
1,929 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure clock selector MC_CGM_ACn_SC is selecting right clock, I assume PLL0 configured for 160Mhz. Or what is your selections?
Then use divider to be consistent with your calculation and clock source selected.

BR, Petr

View solution in original post

0 Kudos
Reply
1 Reply
1,930 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure clock selector MC_CGM_ACn_SC is selecting right clock, I assume PLL0 configured for 160Mhz. Or what is your selections?
Then use divider to be consistent with your calculation and clock source selected.

BR, Petr

0 Kudos
Reply